- Semiconductors & Devices
FOR IMMEDIATE RELEASE No. 3723

Illustration of 200Gbps PIN-PD chip for 800Gbps and 1.6Tbps optical-fiber communication
TOKYO, August 20, 2024 - Mitsubishi Electric Corporation (TOKYO: 6503) announced today that it will begin shipping samples of its new 200Gbps PIN-photodiode (PD) chip for use in next-generation optical transceivers to support 800Gbps and 1.6Tbps fiber communication from October 1 this year. The addition of the new receiver chip to Mitsubishi Electric's optical device lineup will enable existing devices capable of transmitting at 800Gbps/1.6Tbps to newly receive optical data at these same speeds, thereby expanding the communication capacity of optical transceivers, including for high-speed, high-capacity communication in data centers.
The upcoming introduction of the 200Gbps PIN-PD chip for optical reception follows Mitsubishi Electric's launch of a mass-produced chip for optical transmission, the 200Gbps (112Gbaud four-level pulse-amplitude modulation [PAM4]) electro-absorption modulator laser diode (EML), in April this year. Leveraging the company's well-established expertise in optical devices, the newly announced PD chip was developed by minimizing the photoelectric conversion area within a chip structure that integrates backside illumination* and a convex lens.
- *A structure in which the pin junction is on the front side of the semiconductor substrate, allowing incidental light to be received on the opposite (back) side.
Inquiry
Media contact
Customer Inquiries
Related articles
- Semiconductors & Devices