- Research & Development
- Semiconductors & Devices
FOR IMMEDIATE RELEASE No. 3611

Image of the base-stations with before/after amplifiers
TOKYO, June 8, 2023 - Mitsubishi Electric Corporation (TOKYO: 6503) announced today it has developed what is believed to be the world's first* gallium nitride (GaN) power amplifier that achieves a frequency range of 3,400MHz using a single power amplifier, which the company has demonstrated can be used for 4G, 5G and Beyond 5G/6G communication systems operating at different frequencies in a single base station. The amplifier is expected to enable the radio unit (transceiver) to be shared for different communication systems and lead to more power-efficient base stations. Technical details will be presented at the IEEE International Microwave Symposium 2023 this month.
- * According to Mitsubishi Electric research as of June 8, 2023
Inquiry
Media contact
Customer Inquiries
Related articles
- Research & Development
-
Mar 27, 2025
-
Mar 13, 2025
-
Feb 27, 2025
- Semiconductors & Devices