- Semiconductors & Devices
FOR IMMEDIATE RELEASE No. 3559

KD6R1064CXF-NL model in new KD-CXF series
TOKYO, November 30, 2022 - Mitsubishi Electric Corporation (TOKYO: 6503) announced today that its new KD-CXF series of contact image sensors (CISs) equipped with the industry's deepest1 depth of field2 will launch this December beginning with the KD6R1064CXF-NL model. CISs are widely used in manufacturing to inspect product surfaces for scratches, dirt, miscoloring or mispositioning of printed labels, plastic film, etc. Mitsubishi Electric's CIS lineup comprises compactly designed models for space-saving installations that eliminate the need to change production line layouts at points where inspections are most required, thus significantly minimizing installation costs. Also, the image sensor, lens, etc. are built into the CIS unit, eliminating the need for complicated installations and optical adjustments, thereby minimizing maintenance and servicing costs.
Until now, the limitation of a shallow depth of field has made it difficult for CIS units to clearly focus on and accurately inspect objects that have significant surface irregularities or if they are subjected to strong vibration while moving down a production line. The company's existing CIS models are only used to inspect objects with flat surfaces, such as paper and film, and objects not subjected to vibration during inspection.
The KD6R1064CXF-NL model being launched in the new KD series combines an Erecting equal-magnification lens array (rod lens array)3 with unique optical components to improve the depth of field to ±1.8mm, which is more than 3.6 times that of existing products.4 Image reading is clear even if the object has significant surface irregularities or vibrates.
Manufacturing sites are facing increasing market demands for quality while also having to meet needs for labor-saving and automation due to rising labor costs and declining workforces in certain markets. Moreover, manufacturers are looking for ways to reduce the costs of installing, maintaining and servicing inspection equipment. Mitsubishi Electric's new KD-CXF series of CISs will help to satisfy such demands.
- 1As of November 30, 2022, according to Mitsubishi Electric's research into contact image sensor products
- 2Distance in which focus is maintained to read an image clear even when the object deviates from the focal point.
- 3Optical system in which a number of cylindrical lenses are arranged in parallel and the erecting equal-magnification images of each lens are superimposed to form one continuous image.
- 4Mitsubishi Electric's existing KD-AX, MX, CX, CXL and DXL series products
Inquiry
Media contact
Related articles
- Semiconductors & Devices