- Semiconductors & Devices
FOR IMMEDIATE RELEASE No. 3369
TOKYO, September 3, 2020 - Mitsubishi Electric Corporation (TOKYO: 6503) announced today that it will begin shipping samples of its 100Gbps EML (electro-absorption modulator laser) CAN for high-speed, large-capacity optical data transmissions in fifth-generation (5G) mobile base stations on radio access networks on October 1. The new model also supports enhanced manufacturing productivity.
![100Gbps EML CAN (ML770B64)](/mobile0c9a66/sites/news/2020/images/0903-b.jpg)
100Gbps EML CAN (ML770B64)
Sales Schedule
Product | Model | Wavelength | Operating case temperature range | Shipment date |
---|---|---|---|---|
100Gbps EML CAN | ML770B64 | 1310nm | - 40°C to + 95°C | October 1, 2020 |
Mobile communication systems worldwide are being required to handle increasing data communication volume due to the transition from 4G to 5G, the spread of mobile terminals including smartphones and tablets, and the shift of information to the cloud. The expansion of 5G mobile networks will require the transmission of huge volumes of data to/and from base stations in high-speed optical communication networks, which in turn will drive the demand for high-speed, low-power-consumption optical devices. The new 100Gbps EML CAN not only meets these requirements, it also contributes to greater efficiency in manufacturing optical transceivers. The new 100Gbps EML CAN utilizing the industry-standard TO-56 CAN package will be provided for 5G base stations.
Inquiry
Media contact
Customer Inquiries
Related articles
- Semiconductors & Devices
-
Jun 14, 2024
-
Jun 10, 2024
-
Jun 06, 2024