- Semiconductors & Devices
FOR IMMEDIATE RELEASE No. 3323
TOKYO, December 12, 2019, 2019 - Mitsubishi Electric Corporation (TOKYO: 6503) announced today that its lineup of gallium-nitride high-electron-mobility transistors (GaN-HEMTs) for satellite-communication (SATCOM) earth stations will be expanded with the addition of new Ku-band (12-18GHz) 70W and 100W GaN-HEMTs suitable for multi-carrier applications. The 70W-model GaN-HEMT achieves low third-order intermodulation distortion (IMD3)* with a wide offset frequency** of up to 400MHz, which is believed to be the industry's highest level, while the 100W-model GaN HEMT combines unmatched power output with low IMD3 and an offset frequency of up to 200MHz. Mitsubishi Electric will begin shipping samples of both models on January 15.
- *Measure of an amplifier's distortion performance in the case of two-tone signals
- **Frequency difference between two-tone signals, used in IMD3 measurements

GaN HEMTs for Ku-band SATCOM earth stations
Left: MGFK50G3745A (100W) Right: MGFK48G3745A (70W)
The demands for Ku-band satellite communications and satellite news-gathering (SNG) are rapidly growing to support communications during natural disasters and in rural areas where the installation of cable network equipment is difficult. In addition, increasingly large-capacity, high-speed communications have expanded needs for both multi-carrier and single-carrier satellite communications. Mitsubishi Electric's new GaN HEMTs are expected to accelerate the realization of smaller earth stations as well as faster and larger-capacity communications for various needs.
Sales Schedule
Product | Application | Model | Overview | Shipment | ||
---|---|---|---|---|---|---|
Frequency | Saturated output power |
Offset frequency |
||||
Ku-band GaN- HEMTs |
SATCOM earth stations |
MGFK48G3745A | 13.75-14.5GHz | 48.3dBm (70W) |
Up to 400MHz | Jan. 15, 2020 |
MGFK50G3745A | 50.0dBm (100W) |
Up to 200MHz |
Product Features
- 1)Industry-leading wide offset frequency up to 400MHz for large-capacity satellite communication
- The MGFK48G3745A model uses a new matching circuit to deliver an industry-leading wide offset frequency, which is 80 times higher than that of current models, and low IMD3 with a wide offset frequency of up to 400MHz, for large-capacity, high-speed satellite communications, including for multiple carriers.
- 2)Unrivaled output power up to 100W will contribute to downsizing of SATCOM earth stations
- The MGFK50G3745A model uses optimized transistor matching circuits to deliver 100W peak output power and low IMD3 to help downsize SATCOM earth stations by reducing on-board components.
Inquiry
Media contact
Customer Inquiries
Related articles
- Semiconductors & Devices