- Semiconductors & Devices
FOR IMMEDIATE RELEASE No. 3209
TOKYO, September 4, 2018 - Mitsubishi Electric Corporation (TOKYO: 6503) announced today the launch of a 25Gbps EML CAN module supporting high-speed optical data transmission in radio access networks within fifth-generation (5G) mobile base stations. The new module will be on display at the China International Optoelectronic Exposition (CIOE) 2018 in Shenzhen, China, from September 5 to 8, and will be commercially available from November 1.

25Gbps EML CAN (ML760B54)
Sales Schedule
Product | Model | Wavelength | Operating case temperture range |
Shipment date |
25Gbps EML CAN |
ML760B54 | 1270nm, 1310nm |
- 40℃ to + 95℃ | November 1, 2018 |
The introduction of 5G mobile networks will herald the transmission of huge volumes of data and the need for high-speed optical communication networks; this will in turn drive customer demand for high-speed optical devices with low power consumption. The new 25Gbps EML CAN unit addresses these requirements, and will help to improve the productivity and efficiency of customer installations.
Product Features
- 1) Supports high-speed, large-volume mobile networks
- Employs a TO-CAN package delivering 25Gbps EML, an industry first*
- Leverages improved bandwidth of the TO-CAN package
- 2) Reduces power consumption within mobile networks
- Reduces the power consumption of thermo-electric coolers by 40 percent compared to the current FU-411REA model
- 3) Improves customer productivity
- Is compatible with the standard TO-56 CAN package (package size:φ5.6mm)
- Improves the productivity of bi-directional optical modules and transceivers due to a simplified fabrication process
- *According to Mitsubishi Electric as of September 4, 2018
Inquiry
Media contact
Customer Inquiries
Related articles
- Semiconductors & Devices