- Space Systems
FOR IMMEDIATE RELEASE No. 3502
TOKYO, March 24, 2022 - Mitsubishi Electric Corporation (TOKYO: 6503) announced today that it has completed initial verification of the functions and performance of equipment aboard the QZS-1R satellite, which the company built and delivered to the Cabinet Office of Japan and is now in quasi-zenith orbit as the successor to the original Michibiki Quasi-Zenith Satellite (QZS-1).
With Quasi-Zenith Satellite System Services Inc. also having completed testing of related ground systems, the Cabinet Office will begin launching various positioning services via the QZS-1R today.
Mitsubishi Electric, in addition to supporting these services, will continue developing satellite systems that the company intends to provide for forthcoming satellites (QZS-5 to QZS-7) that will support advanced, sustainable, high-precision positioning in Japan.
-
Illustration of QZS-1R
-
QZS-1R logo
Overview of QZS-1R
The QZS-1R was launched on October 26, 2021 from Tanegashima Island in Kagoshima Prefecture. Compared to the first Michibiki satellite, the QZS-1R has improved durability that is expected to extend the satellite's design life by about five years compared to its predecessor. The QZS-1R, together with the QZS-2, 3 and 4 (all launched in 2017), will support positioning, high-precision positioning augmentation and other satellite services.
Name | QZS-1R |
Mass | Dry mass*: approx. 1.6 tons; At launch: approx. 4.0 tons |
Dimensions | Stowed: approx. 5.4m x 2.9m x 2.9m; Wing span: approx. 19m |
Orbit | Quasi-zenith orbit |
Design life | More than 15 years |
- *Dry mass is the satellite mass without propellant.
Inquiry
Media contact
Related articles
- Space Systems
-
Oct 02, 2024
-
Sep 19, 2024
-
Aug 06, 2024