The following are possible areas of application for the Infrared Sensor. With the exception of HVAC, none of these applications have yet been tested and no products are currently under development or available for purchase. Accordingly, there are no claims are made as to the ability of the Infrared Sensor to achieve success in these applications.
Detects patient movement
* : This cannot be used for medical diagnosis.