News Release Archives
Note that the releases are accurate at the time of publication but may be subject to change without notice.
FOR IMMEDIATE RELEASE No. 2754
Mitsubishi Electric to Release Sample TYPE+B J-Series IPMs
New intelligent power modules will strengthen automotive safety and functionality
Tokyo, April 18, 2013 - Mitsubishi Electric Corporation (TOKYO: 6503) announced today it has developed a series of large-capacity intelligent power modules (IPMs) mainly for application in electric and hybrid vehicles. Sample shipments of two J-Series IPM (TYPE+B) models will start August 5 and mass production is expected to begin in 2014.

J-Series IPM (TYPE+B) models will be exhibited at Power Conversion Intelligent Motion (PCIM) Europe 2013 in Nuremberg, Germany on May 14-16.


J-Series IPM (TYPE+B) models will be exhibited at Power Conversion Intelligent Motion (PCIM) Europe 2013 in Nuremberg, Germany on May 14-16.

Power modules for automobiles offer higher reliability than industrial-use modules due to extremely high standards for vehicle safety. Mitsubishi Electric pioneered the mass production of power modules for hybrid vehicles in 1997, and since then the demand for these modules has grown in parallel with the expanding global market for electric and hybrid vehicles.

Sample Products

Features of Sample Products

Sample Products
Series | Package | Model | Specifications | Saturation Voltage (Typ, Ic=Ratings, Tj=25℃) |
Sample Shipment |
J-Series IPM |
TYPE+B | PM500CJG120G | 500A/1200V (6-in-1 package) |
2.0V | Aug. 5, 2013 |
PM800CJG060G | 800A/600V (6-in-1 package) |
1.8V |

Features of Sample Products
1) | Large-capacity IPM for automotive motors
|
||||||
![]() | |||||||
2) | All-in-one IPM for automotive motors
|