BackPrint

News Release Archives

Note that the releases are accurate at the time of publication but may be subject to change without notice.

FOR IMMEDIATE RELEASE No. 2754

Mitsubishi Electric to Release Sample TYPE+B J-Series IPMs

New intelligent power modules will strengthen automotive safety and functionality

Tokyo, April 18, 2013 - Mitsubishi Electric Corporation (TOKYO: 6503) announced today it has developed a series of large-capacity intelligent power modules (IPMs) mainly for application in electric and hybrid vehicles. Sample shipments of two J-Series IPM (TYPE+B) models will start August 5 and mass production is expected to begin in 2014.

J-Series IPM (TYPE+B) models will be exhibited at Power Conversion Intelligent Motion (PCIM) Europe 2013 in Nuremberg, Germany on May 14-16.

J-Series IPM TYPE+B

J-Series IPM TYPE+B

Power modules for automobiles offer higher reliability than industrial-use modules due to extremely high standards for vehicle safety. Mitsubishi Electric pioneered the mass production of power modules for hybrid vehicles in 1997, and since then the demand for these modules has grown in parallel with the expanding global market for electric and hybrid vehicles.

Sample Products
Series Package Model Specifications Saturation Voltage
(Typ, Ic=Ratings, Tj=25℃)
Sample Shipment
J-Series
IPM
TYPE+B PM500CJG120G 500A/1200V
(6-in-1 package)
2.0V Aug. 5, 2013
PM800CJG060G 800A/600V
(6-in-1 package)
1.8V


Features of Sample Products
1) Large-capacity IPM for automotive motors
-J-Series TYPE+B series offers a choice of 600V/800A and 1,200V/500A models.
-Larger current capacity than existing TYPE-B models, but with same footprint area.
-Built-in power supplies for IGBT drive and logic circuits.
2) All-in-one IPM for automotive motors
-Low-loss 3-phase CSTBTTM inverter configuration with built-in control-power supply circuit, optimized IGBT drive & protection circuit, and high-grade isolation photo-couplers.
-High-accuracy analog temperature monitor for chip center.

Inquiry