|
Positioning
|
 |
QZSS (Quasi-Zenith Satellite System) |
Client |
JAXA |
 |
Launch date |
September 11, 2010 |
Launch vehicle |
H-IIA |
Launch site |
Tanegashima Space Center |
Orbit |
Quasi-Zenith Orbit (geosynchronous orbit with inclination of 45 degrees) |
Mass |
approx. 4t (at launch) |
Electrical power |
5,300W |
Design life |
10 years |
Responsibilities |
Prime contractor |
Outline |
QZSS is a constellation of Japan's positioning satellites which will have geosynchronous orbit with inclination of 45 degrees in order to pass near the zenith over Japan, thus providing seamless service irrespective of geographical features. They will significantly improve the accuracy of positioning in areas where signals from GPS Satellites are not fully received due to skyscrapers or canyons. 3 QZS' are needed in order to make sure at least one QZS is at zenith over Japan. |
|