Ground SystemsControl Systems
JAXA Tracking Control for Launch Vehicles
This system consists of a precision radar and telemeter command systems.
The precision radar system can measure the distance and direction of a launch vehicle in real-time with outstanding accuracy. The telemeter command system, which operates at three different frequencies with a single antenna, is capable of monitoring the condition of a rocket and transmitting commands to the rocket. The combination of these two systems creates a highly reliable, top of the line system for tracking control.

Systems delivered by Mitsubishi Electric:
Precision RADAR:
- Takesaki
- Ogasawara
- Masuda
- Miyabaru
Telemeter Command Antenna:
- Uchugaoka
- Masuda
- Ogasawara
Command Antenna:
- Ogasawara
Telemeter Antenna:
- Ogasawara(Under Construction)