- Automotive Equipment
FOR IMMEDIATE RELEASE No. 3469
TOKYO, December 20, 2021 December 29, 2021 - Mitsubishi Electric Corporation (TOKYO: 6503) announced today that it has developed a new concept car, the EMIRAI xS Drive, equipped with near-infrared cameras and radio-wave sensors to monitor the driver and passengers and an Advanced Driver Assistance System (ADAS) to provide adaptive control of the headlights, both of which help to avoid traffic accidents. The new concept car will be exhibited at CES 2022 from this coming January 5 to 8 at the Las Vegas Convention Center in the USA. The company will discontinue the real exhibition due to the expansion of the novel coronavirus (COVID-19).

Rendition of EMIRAI xS Drive
Features
- 1)Monitors drivers and others with near-infrared camera and radio-wave sensor to prevent accidents. etc.
- The system uses an onboard near-infrared camera to detect driver drowsiness or sudden sickness based on facial expressions (closed eyes, open mouth, etc.) and other body information (e.g. pulse and respiration rates). Face-tracking and image-processing technology detect slight variations in skin tone due to changes in heartbeat, even in the presence of vehicle vibrations and/or changes in ambient light. If abnormal physical conditions are detected, the system is capable of suggesting that the driver stop to rest or can even activate an automated emergency-parking function to prevent possible accidents.
- The system also uses the near-infrared camera to detect the presence of occupants and uses the position of a passenger's face and the skeletal points of their upper body to accurately determine body size. Radio waves from a sensor are processed using the signals' reflective and transmissive properties to detect the presence of children in the near-infrared camera's blind spots, such as wrapped in a blanket or down in the footwell. Using this combined information, the system detects with high accuracy if a child is left behind in the vehicle, in which case the system notifies the driver and others nearby.
- The system uses an onboard near-infrared camera to detect driver drowsiness or sudden sickness based on facial expressions (closed eyes, open mouth, etc.) and other body information (e.g. pulse and respiration rates). Face-tracking and image-processing technology detect slight variations in skin tone due to changes in heartbeat, even in the presence of vehicle vibrations and/or changes in ambient light. If abnormal physical conditions are detected, the system is capable of suggesting that the driver stop to rest or can even activate an automated emergency-parking function to prevent possible accidents.
- 2)Supports safer driving at night by controlling headlights adaptively with internal/external sensors
- Mitsubishi Electric's High-Definition Locator (HDL) and Driver Monitoring System (DMS) enable headlight control* to adapt the curve and slope of the road ahead and the driver's direction of view. Areas where the driver is looking, and also potentially dangerous hazards, are brightly illuminated to support safer driving at night.
- *Joint development with Stanley Electric Co., Ltd.
- Further support for intuitive risk-recognition is achieved using the vehicle's external cameras and millimeter-wave radar to issue warnings via 3D sound and road projection, which enables the driver to recognize potential hazards ahead as well as approaching vehicles from behind without having to look.
- Mitsubishi Electric's High-Definition Locator (HDL) and Driver Monitoring System (DMS) enable headlight control* to adapt the curve and slope of the road ahead and the driver's direction of view. Areas where the driver is looking, and also potentially dangerous hazards, are brightly illuminated to support safer driving at night.
Inquiry
Media contact
Related articles
- Automotive Equipment
-
Dec 23, 2024
-
Nov 25, 2024
-
Oct 31, 2024