News Release Archives
Note that the releases are accurate at the time of publication but may be subject to change without notice.
FOR IMMEDIATE RELEASE No. 3104
Mitsubishi Electric to Launch LV100-type X-Series HVIGBT Modules
Top-class current density will contribute increased power output in inverter systems
TOKYO, May 11, 2017 - Mitsubishi Electric Corporation (TOKYO: 6503) announced today that it has launched two new LV100-type X-Series HVIGBT modules sequentially in September. The modules, which will offer the highest power density available on the market, will enable inverter systems to achieve increased power output and efficiency, as well as more flexible configurations and higher reliability. In addition, further line-up of SiC modules is planned in order. Mitsubishi Electric's HVIGBT modules play a vital role in controlling power conversion in industrial electronic systems for railways, power transmission and other large industrial application.
![](/news/images/common/1pix.gif)
The new modules will be exhibited at Power Conversion and Intelligent Motion (PCIM) Europe 2017 in Nuremberg, Germany from May 16 to 18 and PCIM Asia 2017 in Shanghai, China from June 27 to 29.
![](/news/images/common/1pix.gif)
![](/news/images/common/1pix.gif)
The new modules will be exhibited at Power Conversion and Intelligent Motion (PCIM) Europe 2017 in Nuremberg, Germany from May 16 to 18 and PCIM Asia 2017 in Shanghai, China from June 27 to 29.
![](/news/images/common/1pix.gif)
Sales Schedule
Product | Model | Specification | Shipment |
LV100-type X-Series HVIGBT module |
CM450DA-66X | 3.3kV/450A/2in1 | From September 2017 |
CM600DA-66X | 3.3kV/600A/2in1 |
Product Features
1) | Industry-leading power density for increased capacity
|
||||
2) | Easy parallel connection for flexible configurations and capacities
|
||||
3) | New package structure for extra reliability
|