News Release Archives
Note that the releases are accurate at the time of publication but may be subject to change without notice.
FOR IMMEDIATE RELEASE No. 3103
Mitsubishi Electric's Color TFT-LCD Lineup to Add 19.0-inch Projected Capacitive Touch Panel for Industrial Applications
TOKYO, May 8, 2017 - Mitsubishi Electric Corporation (TOKYO: 6503) announced today the launch of a 19.0-inch SXGA color TFT-LCD module, which is equipped with a projected capacitive touch panel utilizing a cover glass of up to 5 millimeters in thickness. Sample sales will begin on June 30 via Mitsubishi Electric offices worldwide. The new module will be presented at the 20th Embedded Systems Expo (ESEC Spring) at the Tokyo Big Sight exhibition complex from May 10 to 12.


The new module will meet increasing industrial demands for extra-thick or glove-operable cover glass. It also enables accurate, multi-touch sensing even when the screen is wet. The combination of these cutting-edge touch capabilities and Mitsubishi Electric's proven TFT-LCD technologies will support diverse applications and installations.
Product Features
1) | Color TFT-LCD with large projected capacitive touch panel for diverse industrial applications
|
||||||||
2) | Projected capacitive touch panel offers superior operability
|
||||||||
3) | Total solution for touch panels
|
Sample Sale Schedule
Product | Model | Display Size |
Resolution | LED Driver | Shipment |
TFT-LCD Module with Projected Capacitive touch panel |
AA190EB02-PCAP | 19.0-inch | SXGA | Provided | June 30, 2017 |
Inquiry
Customer Inquiries
Mitsubishi Electric Corporation