News Release Archives
Note that the releases are accurate at the time of publication but may be subject to change without notice.
FOR IMMEDIATE RELEASE No. 3066
Mitsubishi Electric Develops 3D-model AR Technology for Inspections
AR smart glasses help to reduce workload and confirm data accuracy
TOKYO, November 7, 2016 - Mitsubishi Electric Corporation (TOKYO: 6503) announced today that it has developed a maintenance-support technology using augmented reality (AR) based on a three-dimensional model that enables a technician wearing smart glasses to confirm the order of the inspection on an AR display and then enter the results by voice. The technology helps reduce workload and avoid entry errors because information can be entered by voice, even in noisy environments. The system is expected to be used for a variety of maintenance work, such as inspections of water-treatment plants and building electrical systems




Comparison with Conventional Technology
New technology | Conventional technology | |
Function | AR display based on three-dimensional model | Two-dimensional AR display |
Voice recognition using deep learning | Voice recognition using simple statistical model (Hidden Markov Model) |
|
Performance | Object positioning with max. 1.2 cm error at 60 cm | Object positioning with max. 4.0 cm error at 60 cm |
95 % accuracy at max. 85dbA | 90 % accuracy at max. 85dbA |
Features
1) | Precise, intuitive inspections with reduced workload
|
|
![]() | ||
2) | Voice entry on AR displayed-form is precise and reduces double checking
|
Inquiry
Customer Inquiries
Mitsubishi Electric Corporation