News Release Archives
Note that the releases are accurate at the time of publication but may be subject to change without notice.
FOR IMMEDIATE RELEASE No. 3053
Mitsubishi Electric to Expand Lineup of Ku-band GaN-HEMTs
High output power of new models will help reduce size of satellite earth stations
TOKYO, September 27, 2016 - Mitsubishi Electric Corporation (TOKYO: 6503) announced today that it will expand its lineup of Gallium Nitride High Electron Mobility Transistors (GaN-HEMTs) to include units with 100W and 70W output power for use in satellite earth stations utilizing the Ku-band*. The new 100W GaN-HEMT offers output power that is among the highest currently available, according to Mitsubishi Electric's own research as of September 27. Mitsubishi Electric will begin shipping samples on October 1.
* | Microwave band ranging from 12-18GHz |
The demand for satellite communication is increasing, especially in Ku-band, which enables high-speed communication even under adverse conditions, such as natural disasters, and in areas where construction of communication facilities is difficult. The deployment of transmitter equipment using higher-power GaN-HEMTs has become more common in recent years, particularly in high-speed applications such as satellite news gathering.
![](/news/images/common/1pix.gif)
Mitsubishi Electric is expanding its Ku-band GaN-HEMT lineup to meet this growing demand for higher output power levels with the introduction of its MGFK50G3745 model, boasting an industry-leading output power of 100W, and the 70W output power MGFK48G3745 model.
![](/news/images/common/1pix.gif)
![](/news/images/common/1pix.gif)
Mitsubishi Electric is expanding its Ku-band GaN-HEMT lineup to meet this growing demand for higher output power levels with the introduction of its MGFK50G3745 model, boasting an industry-leading output power of 100W, and the 70W output power MGFK48G3745 model.
![](/news/images/common/1pix.gif)
Product Features
1) | Industry-leading output power contributes to miniaturization
|
||||||
2) | Expands product line-up and meets diverse needs
|
Sale Schedule
Product | Application | Model | Overview | Shipment | ||
Frequency | Saturated output power |
Linear gain |
||||
Ku-band GaN- HEMTs |
Satellite earth stations |
MGFK50G3745 | 13.75-14.5 GHz |
50.0dBm (100W) |
10.0dB | Jan. 1, 2017 |
MGFK48G3745 | 48.3dBm (70W) |
10.0dB | Oct. 1, 2016 |
Inquiry
Customer Inquiries
Mitsubishi Electric Corporation