News Release Archives
Note that the releases are accurate at the time of publication but may be subject to change without notice.
FOR IMMEDIATE RELEASE No. 3011
Mitsubishi Electric to Launch Compact Integrated 100Gbps EML-TOSA
Will support long-haul transmissions and downsizing of 100Gbps communication equipment
TOKYO, March 16, 2016 - Mitsubishi Electric Corporation (TOKYO: 6503) announced today that it will begin shipping a laser diode-transmitter optical subassembly (TOSA) capable of supporting 100Gbps optical transmissions on July 1. The new TOSA, which features four electro-absorption modulators with laser diode (EML) integrated with an optical multiplexer, offers one of most compact EML-TOSA solutions available for IEEE 100GBASE-ER4 applications.

The device will be displayed at the Optical Fiber Communication Conference and Exhibition 2016 (OFC) in Anaheim, California from March 20 to 24.


The device will be displayed at the Optical Fiber Communication Conference and Exhibition 2016 (OFC) in Anaheim, California from March 20 to 24.

In response to the growing need to install communication equipment in increasingly confined spaces, Mitsubishi Electric's new laser-diode TOSA offers 40km transmission capability in one of the industry's smallest footprints, a combination that is expected to help downsize 100Gbps communication facilities and expand high-speed 100Gbps optical transmission networks.


Product Features
1) | High-performance EML for long-distance transmissions
|
||||
2) | Size measuring just 30 percent that of predecessor will help to miniaturize optical transceivers
|
Sales Schedule
Product | Model | Features | Shipment date |
Compact Integrated 100Gbps EML-TOSA |
FU-402REA | - EML with 1.3μm wavelength - LC receptacle |
July 1, 2016 |
Inquiry
Customer Inquiries
Mitsubishi Electric Corporation