News Release Archives
Note that the releases are accurate at the time of publication but may be subject to change without notice.
FOR IMMEDIATE RELEASE No. 2983
Mitsubishi Electric to Launch Can-type Optical Transmitter Module for Mobile Networks
Helps to reduce power consumption of radio access networks
TOKYO, January 20, 2016 - Mitsubishi Electric Corporation (TOKYO: 6503) announced today the coming launch of a 10 Gbps optical transmitter for high-speed, large-volume data transmission between base stations and central offices in radio access networks within mobile telecommunication systems. The module, which comprises an electro-absorption modulator laser (EML) and a transmitter optical sub-assembly (TOSA), reduces fluctuations in optical wavelengths for dense wavelength-division multiplexing (DWDM). Mitsubishi Electric will commercially launch its new EML-TOSA on February 1.
![](/news/images/common/1pix.gif)
The module, which complies with the 10 Gbps Miniature Device Multi Source Agreement (XMD-MSA), features a cylindrical can-type─not box-type─profile suitable for mass production.
![](/news/images/common/1pix.gif)
![](/news/images/common/1pix.gif)
The module, which complies with the 10 Gbps Miniature Device Multi Source Agreement (XMD-MSA), features a cylindrical can-type─not box-type─profile suitable for mass production.
![](/news/images/common/1pix.gif)
In LTE and LTE-Advanced fourth-generation (4G) mobile systems, DWDM has attracted attention as a means of reducing the power consumption of optical transmitter modules that transmit data between base stations and central offices. Mitsubishi Electric's new Can-type EML-TOSA is compatible with DWDM and its TOSA can operate in an industry-leading maximum temperature of up to 95 degrees Celsius.
![](/news/images/common/1pix.gif)
![](/news/images/common/1pix.gif)
Product Features
1) | Reduces power consumption of network equipment
|
||||
2) | Compatible with DWDM and contributes to increased traffic capacity
|
||||
3) | Helps to reduce the size of optical transmission equipment
|
Sales Schedule
Product | Model | Transmission length | Operating case temperture range |
Shipment date |
10 Gbps DWDM Can-type EML-TOSA |
FU-615REA | 25 km | -40℃ to + 95℃ | February 1, 2016 |
Inquiry
Customer Inquiries
Mitsubishi Electric Corporation