News Release Archives
Note that the releases are accurate at the time of publication but may be subject to change without notice.
FOR IMMEDIATE RELEASE No. 2957
Mitsubishi Electric to Build DC Development and Demonstration Facility at Power Distribution System Center in Marugame, Japan
Promoting middle-voltage direct current distribution systems that respond to environmental needs
TOKYO, September 14, 2015- Mitsubishi Electric Corporation announced today that it plans to build a development and demonstration facility for middle-voltage direct current (MVDC*) distribution at its Power Distribution System Center in Marugame, Japan, with operations scheduled to start in April 2016. MVDC distribution reduces electricity loss at delivery, making related technologies increasingly attractive for businesses looking to mitigate environmental impact.
Environmentally conscious distribution systems that combine renewable energy such as solar and wind with an electrical accumulator are growing in popularity. These systems generate DC electricity and then convert it to AC for general use. However, communication devices and digital devices in general have to convert it back to DC. Energy loss will occur when electricity is being converted between AC and DC. MVDC distribution eliminates the DC conversion issue and reduces energy loss, enabling facilities to cut costs by using thinner power cables or transmitting electric power longer distances. This has prompted a reevaluation of DC technology, and Mitsubishi Electric aims to meet the needs of this new DC ecosystem by leveraging their existing DC technologies such as their distribution board for data center energy conservation and their high speed circuit for railway lines. At the same time, the company will use this new facility to develop next-generation MVDC technologies and communicate their value to consumers.
Environmentally conscious distribution systems that combine renewable energy such as solar and wind with an electrical accumulator are growing in popularity. These systems generate DC electricity and then convert it to AC for general use. However, communication devices and digital devices in general have to convert it back to DC. Energy loss will occur when electricity is being converted between AC and DC. MVDC distribution eliminates the DC conversion issue and reduces energy loss, enabling facilities to cut costs by using thinner power cables or transmitting electric power longer distances. This has prompted a reevaluation of DC technology, and Mitsubishi Electric aims to meet the needs of this new DC ecosystem by leveraging their existing DC technologies such as their distribution board for data center energy conservation and their high speed circuit for railway lines. At the same time, the company will use this new facility to develop next-generation MVDC technologies and communicate their value to consumers.
Facility Outline
Location | 8 Horai-cho, Marugame, Kagawa Prefecture, Japan |
Building area | About 180 square meters (gross floor area: about 500 square meters) |
Structure | Three-story steel construction |
Groundbreaking | September 2015 |
Completion | March 2016 |
Operations | From April 2016 |
Investment | About 500 million yen |
Main focus | Commutating devices, solar power generation, wind power generation, electrical accumulators, EMS and DC load systems |
* | Voltage ranges below 1,500V DC as specified by the International Electrotechnical Commission's international standard IEC60364. |
About Power Distribution System Center
Mitsubishi Electric's Power Distribution System Center in Marugame, Kagawa Prefecture, was established in 1979 to manufacture circuit breakers and switchgear. It produced its one millionth circuit breaker in March 2014.
Mitsubishi Electric's Power Distribution System Center in Marugame, Kagawa Prefecture, was established in 1979 to manufacture circuit breakers and switchgear. It produced its one millionth circuit breaker in March 2014.
Inquiry
Customer Inquiries
Mitsubishi Electric Corporation