News Release Archives
Note that the releases are accurate at the time of publication but may be subject to change without notice.
FOR IMMEDIATE RELEASE No. 2940
Mitsubishi Electric to Launch Red Laser Diode for Projectors
Emits industry-leading output power
TOKYO, June 24, 2015- Mitsubishi Electric Corporation announced today that it will launch a 638-nanometer-(nm)-wavelength red laser diode (LD) offering pulse operation output power of 2.5 W, the world's highest level among 638-nm LDs used as light sources for projectors. Sales will begin this September 1. The 638-nm red laser light and highly efficient operation of the LD contributes to the laser projectors with the wide color expression range and low power consumption.
Product Features
1) | Unprecedented output power of 2.5 W at 638 nm under pulse operation due to improved LD structure
|
||||||||||
2) | Wide operational temperature range thanks to new package
|
Inquiry
Customer Inquiries
Mitsubishi Electric Corporation