News Release Archives
Note that the releases are accurate at the time of publication but may be subject to change without notice.
FOR IMMEDIATE RELEASE No. 2933
Mitsubishi Electric to Ship Samples of New IGBT Module T Series with Seventh-generation IGBT
Expanded lineup will contribute to low power loss and high reliability of industrial equipment
TOKYO, May 19, 2015- Mitsubishi Electric Corporation announced today that it would begin shipping samples of its new T series power semiconductor modules featuring seventh-generation insulated-gate bipolar transistors (IGBTs), comprising three different packages and 48 models in total. The new modules realize improved power loss and reliability for general-purpose inverters, elevators, uninterruptible power supplies (UPS) and other industrial equipment. Sample shipments will begin June 30.

The modules will be exhibited at major trade shows including Power Conversion Intelligent Motion (PCIM) Europe 2015 in Nuremberg, Germany from May 19 to 21, MOTORTECH JAPAN 2015 during TECHNO-FRONTIER 2015 in Japan from May 20 to 22, and PCIM Asia 2015 in China from June 24 to 26.


The modules will be exhibited at major trade shows including Power Conversion Intelligent Motion (PCIM) Europe 2015 in Nuremberg, Germany from May 19 to 21, MOTORTECH JAPAN 2015 during TECHNO-FRONTIER 2015 in Japan from May 20 to 22, and PCIM Asia 2015 in China from June 24 to 26.

Product Features
1) | Reduced power loss thanks to seventh-generation IGBT and seventh-generation diode
|
||||||||
2) | Reliability of de facto standard package are improved by latest package technology
|
Sample Shipments
Package | Voltage Rating | Current Rating | Shipment |
NX-type Solder Pin Package |
650V | 100, 150, 200, 300, 450, 600A | From June 30 |
1200V | 100, 150, 200, 225, 300, 450, 600, 1000A | ||
NX-type Press Fit Pin Package |
650V | 100, 150, 200, 300, 450, 600A | |
1200V | 100, 150, 200, 225, 300, 450, 600, 1000A | ||
Standard-type Package |
650V | 100, 150, 200, 300, 400, 600A | |
1200V | 100, 150, 200, 300, 450, 600A |