News Release Archives
Note that the releases are accurate at the time of publication but may be subject to change without notice.
FOR IMMEDIATE RELEASE No. 2928
Mitsubishi Electric to Launch DIPIPM+ Series
Smaller, simpler design for inverter systems in air conditioners and industrial applications
TOKYO, May 7, 2015 - Mitsubishi Electric Corporation announced today the launch of DIPIPM+, new models in its DIPIPMTM series of inverter applications featuring loading converter and brake circuits for reduced design load and size. Sales begin May 29.

The new models will be exhibited at major trade shows including Power Conversion Intelligent Motion (PCIM) Europe 2015 in Nuremberg, Germany from May 19 to 21, MOTORTECH JAPAN 2015 during TECHNO-FRONTIER 2015 in Japan from May 20 to 22, and PCIM Asia 2015 in China from June 24 to 26.

Mitsubishi Electric commercialized its first DIPIPM transfer-mold intelligent power module in 1997, the beginning of its ongoing contributions to miniaturization and energy savings in inverter systems. DIPIPM has contributed to miniaturization and energy-savings in inverter systems. To achieve more compact and simpler design, Mitsubishi Electric has developed DIPIPM+ that has inverter, converter and brake circuit with one package.


The new models will be exhibited at major trade shows including Power Conversion Intelligent Motion (PCIM) Europe 2015 in Nuremberg, Germany from May 19 to 21, MOTORTECH JAPAN 2015 during TECHNO-FRONTIER 2015 in Japan from May 20 to 22, and PCIM Asia 2015 in China from June 24 to 26.

Mitsubishi Electric commercialized its first DIPIPM transfer-mold intelligent power module in 1997, the beginning of its ongoing contributions to miniaturization and energy savings in inverter systems. DIPIPM has contributed to miniaturization and energy-savings in inverter systems. To achieve more compact and simpler design, Mitsubishi Electric has developed DIPIPM+ that has inverter, converter and brake circuit with one package.

Product Features
1) | Inverter, converter and brake circuits in one package for inverter systems
|
||||||
2) | Downsizing and simpler design for inverter systems
|
Sale Schedule
* Does not include a brake circuit
Series | Model | Specification | Shipment |
DIPIPM+ | PSS05MC1FT | 5A/1200V | June 30, 2015 |
PSS10MC1FT | 10A/1200V | ||
PSS15MC1FT | 15A/1200V | ||
PSS25MC1FT | 25A/1200V | May 29, 2015 | |
PSS35NC1FT* | 35A/1200V | June 30, 2015 | |
PSS50MC1F6 | 50A/600V |