News Release Archives
Note that the releases are accurate at the time of publication but may be subject to change without notice.
FOR IMMEDIATE RELEASE No.2893
Mitsubishi Electric to Launch Power Semiconductor Modules for 3-level Inverter
Enhanced low-power consumption and miniaturization for large-capacity industrial equipment
TOKYO, December 25, 2014-Mitsubishi Electric Corporation (TOKYO: 6503) announced today a new family of power semiconductor modules optimized for 3-level inverters that will enhance low-power consumption and size reduction for large-capacity industrial equipment in the 125kW-500kW class and above. Sales will begin in June 2015.


Product Features
1) | About 30% reduction in power consumption owing to 3-level control
|
||||||
2) | Low inductance due to new packages
|
||||||
3) | Lineup offers both downsizing and diverse circuit configurations for inverters
|
Sales Schedule
Product | Model | Specification | Shipment |
Power semiconductor modules for 3-level inverter |
CM400ST-24S1 | 400A/1200V 4in1, IGBT module | June, 2015 |
CM1400HA-24S | 1400A/1200V 1in1, IGBT module | July,2015 | |
RM1400HA-24S | 1400A/1200V 1in1, Diode module | ||
CM1000HA-34S | 1000A/1700V 1in1, IGBT module | August, 2015 | |
CM500C2Y-24S | 500A/1200V 2in1 Emitter common, IGBT module |