News Release Archives
Note that the releases are accurate at the time of publication but may be subject to change without notice.
FOR IMMEDIATE RELEASE No.2862
Mitsubishi Electric to Launch 3.6V High-power MOSFET for Commercial Two-way Radio Devices
TOKYO, August 28, 2014 - Mitsubishi Electric Corporation (TOKYO: 6503) announced today that from September 1 it will begin shipping samples of its model RD04LUS2 high-power metal-oxide semiconductor field-effect transistor (MOSFET), which is designed for use in high-frequency power amplifiers of commercial two-way radio devices. The model offers industry-leading 4W output when using a 3.6V Li-ion 1-cell battery. Mitsubishi Electric will initially produce 200,000 units per month.

While the popularization of mobile phones has led to 3.6V Li-ion batteries costing less than traditional 7.2V batteries, the need for a higher-power MOSFET arose because lower-voltage batteries decrease the MOSFET's output power. Mitsubishi Electric has now met this demand with its new MOSFET, which offers unmatched 4W output power using a 3.6V battery.

Features
1) | Industry's highest power output
|
||||
2) | Top-level 65% drain efficiency
|
Inquiry
Customer Inquiries
Mitsubishi Electric Corporation