BackPrint

News Release Archives

Note that the releases are accurate at the time of publication but may be subject to change without notice.

FOR IMMEDIATE RELEASE No.2850

Mitsubishi Electric to Launch 1,200V Large DIPIPM Ver.6 and 1,200V Mini DIPIPM

Smaller, more efficient power modules for air conditioners and industrial applications

TOKYO, June 30, 2014 - Mitsubishi Electric Corporation (TOKYO: 6503) announced today the launch of its 1,200V large transfer-mold dual in-line package intelligent power module (DIPIPMTM) Ver.6 and 1,200V Mini DIPIPM using sixth-generation IGBT chips featuring the carrier-stored trench-gate bipolar transistor (CSTBTTM) structure. Both modules reduce the power consumption, size and weight of inverter systems for motors used in air conditioners and industrial applications. Sales begin September 30.
The new models will be exhibited at MOTORTECH JAPAN 2014 during TECHNO-FRONTIER 2014 at Tokyo Big Sight in Japan from July 23 to 25.

1,200V Large DIPIPM Ver.6 (5A-50A)

1,200V Large DIPIPM Ver.6 (5A-50A)

1,200V Mini DIPIPM (5A&10A)

1,200V Mini DIPIPM (5A&10A)

Product Features
1) Reduced power consumption and simpler design for inverter systems
-Sixth-generation IGBT chips featuring the CSTBT structure enable power loss to be reduced by about 10% compared to Mitsubishi Electric's existing Large DIPIPM products (Large DIPIPM Ver.4 series, 5A-35A).
-Reduced external components thanks to built-in bootstrap diode (BSD) with current limit resistor.
-Reduced heat dissipation by improving the accuracy of temperature detection output.
2) Downsizing and weight reduction with Mini DIPIPM package: 1,200V Mini DIPIPM
-By employing a Mini DIPIPM package for the first time in a 1,200V product, the profile (31.0 x 52.5mm) was reduced about 34% compared with Mitsubishi Electric's existing Large DIPIPM Ver.4 series (31.0 x 79.0mm).
Sale Schedule
Series Model Specification Shipment
1,200V Large
DIPIPM
Ver.6
PSS05SA2FT 5A / 1200V Sept. 30, 2014
PSS10SA2FT 10A / 1200V
PSS15SA2FT 15A / 1200V
PSS25SA2FT 25A / 1200V
PSS35SA2FT 35A / 1200V
PSS50SA2FT 50A / 1200V
1,200V Mini
DIPIPM
PSS05S72FT 5A / 1200V
PSS10S72FT 10A / 1200V

Inquiry