BackPrint

News Release Archives

Note that the releases are accurate at the time of publication but may be subject to change without notice.

FOR IMMEDIATE RELEASE No. 2846

Mitsubishi Electric's Compact Wind Lidar Approved by Dutch Energy Body

TOKYO, May 28, 2014 - Mitsubishi Electric Corporation (TOKYO: 6503) announced today that the Energy research Centre of the Netherlands (ECN) has conducted tests to validate and subsequently approve Mitsubishi Electric's compact wind lidar as complying with European wind measurement standards. The lidar (portmanteau of "light" and "radar") is a remote sensing apparatus that projects a laser beam and then evaluates the reflected light to measure wind speed.

Fig 1:Rendition of lidar in the Field


Fig 1:Rendition of lidar in the Field

Fig 2:Compact lidar for wind monitoring


Fig 2:Compact lidar for wind monitoring

Fig 3:Meteorological mast


Fig 3:Meteorological mast

Meteorological masts, which are used conventionally to assess local wind prior to constructing a wind farm, only measure wind at fixed points. Also, the growing size of commercial turbines is requiring increasingly taller masts, which is contributing to higher construction costs for meteorological masts.

Mitsubishi Electric's lidar, which uses a laser beam safe for human eyes, can measure wind remotely at multiple altitudes for accurate assessment and prediction of wind-turbine power generation. It also eliminates the need for costly meteorological masts.

Features of Compact Wind Lidar
1) Improved environmental tolerance for diverse operation
- Increased tolerance to extreme environmental conditions, including water resistance to IP67 and temperatures down to -20 degrees Celsius.
-Motion compensation for offshore use to support floating wind turbines.
2) Reduced power consumption and small profile for easy operation
-User friendly weight of under 60 kg and power consumption of less than 100W.
3) Third-party validation of performance by ECN
-Data error less than 1% in comparison to standard IEC cup anemometer.
-Complies with lidar specifications for NORSEWInD, a large European project on offshore wind atlas.
-Data availability during operation is above 95% (accepted by ECN as reasonable).
Future Plans
Mitsubishi Electric will enter the global lidar market by launching commercial sales of its compact wind lidar this June. As the International Energy Agency advances towards international standards for lidars, Mitsubishi Electric looks forward to supplying advanced, reliable lidars worldwide for the further growth and development of wind power as a sustainable energy resource.

Inquiry