BackPrint

News Release Archives

Note that the releases are accurate at the time of publication but may be subject to change without notice.

FOR IMMEDIATE RELEASE No. 2844

Mitsubishi Electric Develops ALOS-2 Satellite System

For disaster monitoring, environmental protection, resource exploration and forest monitoring

TOKYO, May 23, 2014 - Mitsubishi Electric Corporation (TOKYO: 6503) announced today that it has completed its development of the ALOS-2:DAICHI-2 advanced land-observation satellite based on a contract awarded to the company by the Japan Aerospace Exploration Agency (JAXA) in 2009. Mitsubishi Electric will provide the spacecraft, sensor and ground systems, including data processing, and will confirm operation after the ALOS-2 satellite system is launched from Tanegashima Space Center on May 24.

ALOS-2, a follow-on mission of its predecessor ALOS satellite, is equipped with the world's most advanced L-band Synthetic Aperture Radar (SAR) for improved resolution and wider observation range than ALOS. It is expected to contribute significantly to earth observations in terms of disaster monitoring, environmental protection, resource exploration and forest monitoring.

Mitsubishi Electric, a leading manufacturer contributing to space research and development in Japan, has participated in more than 450 domestic and international satellite projects as either the prime contractor or a major subcontractor. The company has developed and delivered numerous earth-observation satellite systems and observation sensors to JAXA and other space-related governmental institutions and agencies. Recently, Mitsubishi Electric was selected as the contractor to supply JAXA with the Greenhouse Gases Observing SATellite-2 (GOSAT-2) satellite system, which the company is now developing.

Going forward, Mitsubishi Electric will continue to contribute to Japanese earth-observation satellite systems as a leading manufacturer in fields ranging from security to the environment.
Rendering of ALOS-2 in Orbit

Rendering of ALOS-2 in Orbit

ALOS-2 at Tanegashima Space Center

ALOS-2 at Tanegashima Space Center

ALOS-2 Overview
Orbital altitude 628 km (sun-synchronous sub-recurrent orbit)
Mass Approx. 2 tons
Design life 5 years (target life of 7 years)
Observation sensor L-band Synthetic Aperture Radar (1.2 GHz band)
Observation Modes   ALOS-2
L-band Synthetic Aperture Radar
ALOS
L-band Synthetic Aperture Radar
Spotlight
Resolution :1 - 3 m  
Swath :25 km  
-
Strip map
Resolution :3, 6 or 10 m
Swath :50, 50 or 70 km
Resolution :10 or 20 m
Swath :70 km
Scan SAR
Resolution :100 or 60 m
Swath :350 or 490 km
Resolution :100 m
Swath :250 - 350 km

Inquiry