News Release Archives
Note that the releases are accurate at the time of publication but may be subject to change without notice.
FOR IMMEDIATE RELEASE No.2806
Mitsubishi Electric to Add Two Touch Panels to Lineup of Color TFT-LCD Modules
TOKYO, December 3, 2013 - Mitsubishi Electric Corporation (TOKYO: 6503) announced today the launch of 8.4-inch XGA and 10.4-inch SVGA color TFT-LCD modules with projected capacitive touch panels offering excellent visual clarity and durable cover glass. Sales will begin on December 3 through Mitsubishi Electric offices worldwide ("http://www.mitsubishielectric.com/semiconductors/)Initial production has been set at 2,000 units per month for each new model.

The two modules will expand the options in Mitsubishi Electric's color TFT-LCD module lineup of high-quality touch-panel screens to 12, available in sizes from 6.5 to 19.0 inches.


The two modules will expand the options in Mitsubishi Electric's color TFT-LCD module lineup of high-quality touch-panel screens to 12, available in sizes from 6.5 to 19.0 inches.

Widely applicable and highly reliable touch-panel solutions | |
![]() |
TFT-LCD, PCAP touch panel, touch controller and driver software in 8.4" and 10.4" versions for factory automation, medical equipment and measuring instrumentation. |
![]() |
Factory-installed TFT-LCD, PCAP touch panel, cover glass and touch controller achieve excellent reliability. |
![]() |
Options for diverse operability, such as optical bonding (resin bonding between TFT-LCD module, touch-panel sensor and cover glass) for clear images in bright environments, tempered cover glass and anti-reflection/anti-smudge surface treatments. |
![]() |
Excellent visual clarity combined with tactile operation via cover glass | |
![]() |
Proprietary detective processing for smooth, accurate response to finger movements, even when gloved. |
![]() |
Ultra-thin, highly conductive sensor lines with proprietary TFT array technologies for excellent clarity. |
![]() |

Display Size | Resolution | Model | |
4:3 | 6.5-inch | VGA | AA65VE11-PCAP |
8.4-inch | SVGA | AA084SD11-PCAP | |
8.4-inch | XGA | AA084XE11-PCAP | |
10.4-inch | SVGA | AA104SL12-PCAP | |
10.4-inch | XGA | AA104XF12-PCAP | |
12.1-inch | XGA | AA121XN11-PCAP | |
15.0-inch | XGA | AA150XT11-PCAP | |
5:4 | 19.0-inch | SXGA | AA190EA01-PCAP |
Wide | 7.0-inch | WVGA | AA070ME11-PCAP |
9.0-inch | WXGA | AA090TB01-PCAP | |
10.6-inch | WXGA | AA106TA01-PCAP | |
12.1-inch | WXGA | AA121TD11-PCAP |
Inquiry
Customer Inquiries
Mitsubishi Electric Corporation