News Release Archives
Note that the releases are accurate at the time of publication but may be subject to change without notice.
FOR IMMEDIATE RELEASE No.2801
Mitsubishi Electric to Launch Ku-band Low-noise GaAs HEMT
Simplifies production and improves performance of direct broadband satellite receiver modules
TOKYO, November 19, 2013- Mitsubishi Electric Corporation (TOKYO: 6503) announced today it will launch a gallium arsenide (GaAs) high-electron mobility transistor (HEMT), the MGF4937AM, as a low-noise amplifier for receiver modules in direct broadband satellites (DBS) and very small aperture terminals (VSAT). Offering the world's lowest noise-figure performance among fully molded package products, Mitsubishi Electric's new GaAs HEMT will simplify the manufacture and improve the performance of receiver module systems. Shipments will begin on December 20 at an initial production volume of four million units per month. Mitsubishi Electric will exhibit MGF4937AM GaAs HEMT at 2013 Microwave Workshops& Exhibition (MWE 2013) in PACIFICO YOKOHAMA, Japan from November 27 to 29.


The market for wireless communication systems created with satellites is growing rapidly, mainly in developing countries because they can be deployed at lower costs than wired systems created with optical fiber networks. As such, demands are increasing for DBS and VSAT receiver modules that offer both improved noise performance and simplified manufacturing. Conventionally, hollow-type package transistors are generally used in first-stage low-noise amplifiers (LNA) due to their strong noise performance, but this complicates assembly.

Mitsubishi Electric's MGF4937AM GaAs HEMT, however, improves the transistor structure and optimizes packaging while achieving noise performance that is unsurpassed for a fully molded package and almost the equal of hollow-type packages.

Product Features

Other Features
Recommended bias conditions: VDS=2V, ID=10mA
Minimum noise figure (NF): 0.37dB (f=12GHz, typical)
Associated gain (Gs): 13.0dB (f=12GHz, typical)

Environmental awareness
MGF4937AM GaAs HEMT is compliant with the European Restriction of the use of certain Hazardous Substances in electrical and electronic equipment (RoHS).

Mitsubishi Electric's MGF4937AM GaAs HEMT, however, improves the transistor structure and optimizes packaging while achieving noise performance that is unsurpassed for a fully molded package and almost the equal of hollow-type packages.

Product Features
1) | Lowest noise performance among fully molded package products Minimum noise figure (NF) of 0.37dB, which is 0.08dB less than conventional fully molded package products, contributing to higher performance in receiver modules. |
||||
2) | Standard 4pin fully molded package
|

Other Features
Recommended bias conditions: VDS=2V, ID=10mA
Minimum noise figure (NF): 0.37dB (f=12GHz, typical)
Associated gain (Gs): 13.0dB (f=12GHz, typical)

Environmental awareness
MGF4937AM GaAs HEMT is compliant with the European Restriction of the use of certain Hazardous Substances in electrical and electronic equipment (RoHS).
Inquiry
Customer Inquiries
Mitsubishi Electric Corporation