BackPrint

News Release Archives

Note that the releases are accurate at the time of publication but may be subject to change without notice.

FOR IMMEDIATE RELEASE No. 2775

Mitsubishi Electric to Expand Lineup of Color TFT-LCD Modules with Projected Capacitive Touch Panels for Industrial Applications

TOKYO, July 25, 2013 - Mitsubishi Electric Corporation (TOKYO: 6503) announced today the launch of 15-inch XGA and 19-inch SXGA color TFT-LCD modules with projected capacitive touch panels that enable intuitive operation. Sales will begin on August 23 at Mitsubishi Electric offices worldwide (www.MitsubishiElectric.com/semiconductors/). Initial production has been set at 1,000 units per month for the 15-inch model and 500 units per month for the 19-inch model.

The 19-inch module with projected capacitive touch panel will be presented at IPC & Embedded Expo 2013 in Shenzhen, China from August 1-3 and International Touch Panel and Optical Film Exhibition 2013 in Taipei, Taiwan from August 28-30.

The two additions to Mitsubishi Electric's color TFT-LCD module lineup have larger screens and offer additional options for a broader range of industrial applications of high quality touch-panel screens compared to existing XGA modules ranging from 6.5 to 12.1 inches and WXGA modules ranging from 9.0 to 10.6 inches.

AA150XT11-PCAP / AA190EA01-PCAP
Highly reliable and widely applicable touch-panel solutions
- Wide range of solutions, including TFT-LCD, PCAP touch panel, touch controller and driver software, for diverse industrial applications.
- Factory-installed TFT-LCD, PCAP touch panel, cover glass and touch controller for excellent reliability.
- Multiple options, such as tempered cover glass and anti-reflection/anti-smudge surface treatments, for diverse operational environments.
Excellent visual clarity combined with tactile operation via cover glass
- Proprietary detective processing for smooth, accurate response to finger movements, even gloved fingers.
- Ultra-thin, highly conductive sensor lines with proprietary TFT array technologies for excellent clarity.


Lineup of color TFT-LCD modules with projected capacitive touch panel (new models in bold)
Display Size Resolution Model
4:3 6.5-inch VGA AA65VE11-PCAP
8.4-inch SVGA AA084SD11-PCAP
10.4-inch XGA AA104XF12-PCAP
12.1-inch XGA AA121XN11-PCAP
15.0-inch XGA AA150XT11-PCAP
5:4 19.0-inch SXGA AA190EA01-PCAP
Wide 9.0-inch WXGA AA090TA01-PCAP
10.6-inch WXGA AA106TA01-PCAP

Inquiry