News Release Archives
Note that the releases are accurate at the time of publication but may be subject to change without notice.
FOR IMMEDIATE RELEASE No.2763
Mitsubishi Electric to Release Sample J1-Series Power Modules
New compact-package power modules for electric and hybrid vehicles
Tokyo, May 13, 2013 - Mitsubishi Electric Corporation (TOKYO: 6503) announced today its new J1-Series power modules featuring a compact 6-in-1 package mainly for use in electric and hybrid vehicles. Sample shipments of two J1-Series modules will start on September 30.

J1-Series power module samples will be exhibited at Power Conversion Intelligent Motion Europe 2013, which will be held in Nuremberg, Germany from May 14 to 16.


J1-Series power module samples will be exhibited at Power Conversion Intelligent Motion Europe 2013, which will be held in Nuremberg, Germany from May 14 to 16.

J1-Series power modules (Above package may be changed without notice)

Power modules for automobiles must deliver higher reliability than industrial-use modules due to the extremely high standards for vehicle safety. Mitsubishi Electric pioneered the mass production of power modules for hybrid vehicles in 1997, and since then the demand for these modules has grown in parallel with the expanding global market for electric and hybrid vehicles. The new J1-Series power modules feature compact package with small footprint, low power loss and high reliability for use in the inverters of electric and hybrid vehicles. Mass production is expected to begin in 2015.

Sample Products
Series | Model | Specifications | Saturation Voltage (Typ, Ic=Ratings, Tj=25℃) |
Start of Sample Shipments |
J1-Series | CT600CJ1A060 | 650V/600A (6-in-1 package) |
1.4V | Sep. 30, 2013 |
CT400CJ1A090 | 900V/400A (6-in-1 package) |
1.7V |

Features of Sample Products
1) | Extra-compact package for automotive inverters
|
||||
![]() | |||||
2) | Low power loss and high reliability for automotive motors
|