News Release Archives
Note that the releases are accurate at the time of publication but may be subject to change without notice.
FOR IMMEDIATE RELEASE No. 2746
Mitsubishi Electric Completes Expansion of Satellite Production Facility
Will help facilitate use of space for new infrastructure and global production
TOKYO, March 22, 2013 - Mitsubishi Electric Corporation (TOKYO: 6503) announced today that it has completed expansion of the satellite production facility at the company's Kamakura Works in Kamakura, Japan. Completed today, the upgraded facility doubles Mitsubishi Electric's annual satellite production capacity to eight satellites, the largest among all facilities operated by Japanese satellite manufacturers.
Mitsubishi Electric has delivered a variety of satellites that now support daily life, including the meteorological satellite Himawari-7, the first Japan-made commercial communications satellite Superbird-C2 and the Quasi-Zenith Satellite-1 MICHIBIKI, which provides location-information services. Currently, the company is developing the Himawari-8, Himawari-9 and ALOS-2 satellites, the last of which will succeed the DAICHI in gathering disaster-related data in areas affected by large-scale natural disasters such as the Great East Japan Earthquake of 2011.


Newly upgraded satellite production facility

The global satellite market is showing increasing demand for communication and other purposes. In addition, Japan's Basic Plan for Space Policy, announced on January 25 as the nation's space plan for the five fiscal years beginning April 2013, includes expanded use of space for telecommunications, broadcasting, positioning and remote sensing purposes that will contribute to improved quality of life.
![]() Mitsubishi Electric looks forward to operating its manufacturing facilities to help develop and manufacture satellites that further enrich daily life. |
![]() Upgraded satellite production facility at Mitsubishi Electric's Kamakura Works |

Newly upgraded satellite production facility
Location | Kamakura, Kanagawa Prefecture, Japan | ||||
Structure | 30.25 m in height, six -story RC structure | ||||
Building area | 2,183 ㎡ | ||||
Floor area | 7,817 ㎡ (total floor area of 23,886 ㎡ including existing facilities) | ||||
Main products |
|
||||
Production capacity | 8 large satellites/year (including existing facilities) | ||||
Investment | Approximately 3 billion yen | ||||
Green measures | 66kW solar-powered system, heat pump air-conditioning system, 900 LED lights and energy-management system |
Inquiry
Customer Inquiries
Mitsubishi Electric Corporation