News Release Archives
Note that the releases are accurate at the time of publication but may be subject to change without notice.
FOR IMMEDIATE RELEASE No. 2738
Mitsubishi Electric to Launch 17.5-inch Color TFT-LCD Module
TOKYO, March 6, 2013 - Mitsubishi Electric Corporation (TOKYO: 6503) announced today it will launch a 17.5-inch wide-XGA, color TFT-LCD module for industrial applications such as POS terminals, factory line displays and others. This model features the unprecedented combination of a super-wide 170-degree viewing angle (both horizontally and vertically), 1000:1 high contrast ratio, -20 to 70 degree Celsius operational temperature range and 100,000 standard hours of LED backlight life. Sales will begin April 1 through Mitsubishi Electric global offices. (www.MitsubishiElectric.com/bu/tft_lcd/network).


The new TFT-LCD module meets increasing market demands for high-contrast, wide viewing angle modules that can be used in extreme operational temperatures for flexible application and installation. With the launch, Mitsubishi Electric will increase its lineup of super wide viewing angle modules up to 14. Features of the new module are as follows:


Super-wide viewing angle, high brightness & contrast, and vivid color
|
||||
![]() |
||||
Long-life backlight through use of white light-emitting diodes (LED)
|
||||
![]() |
||||
Wide-range operational temperature range
|
||||
![]() |
||||
Environmental awareness
|
Inquiry
Customer Inquiries
Mitsubishi Electric Corporation