News Release Archives
Note that the releases are accurate at the time of publication but may be subject to change without notice.
FOR IMMEDIATE RELEASE No. 2736
Mitsubishi Electric to Launch MOSFET-type Super-mini DIPIPM
Contributes to reduced power consumption, miniaturization and lower cost of small-capacity motors for refrigerators, other products
TOKYO, February 18, 2013 - Mitsubishi Electric Corporation (TOKYO: 6503) announced today it will launch a transfer-mold-type, super-mini dual inline package intelligent power module (DIPIPM) primarily used for inverter drive systems of small-capacity motors in refrigerators and other consumer appliances. The module uses a metal oxide semiconductor field effect transistor (MOSFET) switching device featuring low power-on voltage in low current regions. Sales will begin on March 1.
![](/news/images/common/1pix.gif)
With optimized low-loss-drive ICs and a high-heat dissipation design, the module will help to reduce power consumption, advance miniaturization and lower the cost of inverter systems for small-capacity motor drive applications.
![](/news/images/common/1pix.gif)
![](/news/images/common/1pix.gif)
With optimized low-loss-drive ICs and a high-heat dissipation design, the module will help to reduce power consumption, advance miniaturization and lower the cost of inverter systems for small-capacity motor drive applications.
![](/news/images/common/1pix.gif)
Product Features
![](/news/images/common/1pix.gif)
Sale Schedule
![](/news/images/common/1pix.gif)
Main Specifications
![](/news/images/common/1pix.gif)
In 1997, Mitsubishi Electric first commercialized its DIPIPM transfer-mold-type intelligent power module, which has contributed greatly to miniaturization and energy-savings in inverter systems. The technology has gained increased importance because annual power consumption has become an important index of energy-saving performance in consumer appliances, such as refrigerators. Needs are increasing for reducing loss in rated power, and also in low current regions where a high percentage of power use is concentrated.
![](/news/images/common/1pix.gif)
DIPIPM is a registered trademark of Mitsubishi Electric.
Reduced power consumption in small-capacity inverter systems
|
|||||||
![]() |
|||||||
High reliability through high-heat dissipation structure
|
|||||||
![]() |
|||||||
Cost reduction and miniaturization of final product
|
![](/news/images/common/1pix.gif)
Sale Schedule
Model | Specification | Shipment date |
PSM03S93E5/-A/-C | 3A/500V | March 1, 2013 |
PSM05S93E5/-A/-C | 5A/500V |
![](/news/images/common/1pix.gif)
Main Specifications
Model | PSM03S93E5/-A/-C | PSM05S93E5/-A/-C |
Specification | 3A/500V | 5A/500V |
Dimensions | 24 x 38 x 3.5 mm (same as super-mini DIPIPM) | |
Built-in Chips | MOSFET x 6 forming a three-phase bridge, HVIC x 1, LVIC x 1and Bootstrap Diode x 3 |
|
Functions | Protection against short circuits, control power-supply undervoltage and over-heating (LVIC monitoring ); and error output |
|
Others | Divided-source-type N-side MOSFET |
![](/news/images/common/1pix.gif)
In 1997, Mitsubishi Electric first commercialized its DIPIPM transfer-mold-type intelligent power module, which has contributed greatly to miniaturization and energy-savings in inverter systems. The technology has gained increased importance because annual power consumption has become an important index of energy-saving performance in consumer appliances, such as refrigerators. Needs are increasing for reducing loss in rated power, and also in low current regions where a high percentage of power use is concentrated.
![](/news/images/common/1pix.gif)
DIPIPM is a registered trademark of Mitsubishi Electric.