News Release Archives
Note that the releases are accurate at the time of publication but may be subject to change without notice.
FOR IMMEDIATE RELEASE No. 2705
Mitsubishi Electric to Launch Highly Operable & Accurate New CNC Series - MITSUBISHI CNC E70 Series -
Tokyo, October 30, 2012 - Mitsubishi Electric Corporation (TOKYO: 6503) announced today the launch of a new line of computerized numerical controllers (CNC), the MITSUBISHI CNC E70 Series, which extends the company's tradition of extra-operable and accurate high-end CNCs for industrial production. Sales will begin on December 3, 2012 and prices will be available by quotation. The company expects to produce 3,000 units per month.

The E70 Series, which offers world-class ease of use, high speed and accuracy, and reduced takt time, will be showcased at the 26th Japan International Machine Tool Fair (JIMTOF 2012) at Tokyo Big Sight in Japan from November 1-6.


The E70 Series, which offers world-class ease of use, high speed and accuracy, and reduced takt time, will be showcased at the 26th Japan International Machine Tool Fair (JIMTOF 2012) at Tokyo Big Sight in Japan from November 1-6.

Precise mass production of automobiles and electronics requires machine tools that achieve exceptional accuracy and productivity, including through the incorporation of highly operable CNCs capable of high-capacity operation. The rising use of factory automation, particularly in China, Korea, Taiwan and emerging countries such as Brazil and India, has triggered increased demand for CNC machine tools.

Main Features

Specifications

Main Features
Simple operability for stress-free operations
|
|||||||||
![]() |
|||||||||
High-accuracy, nanometer-increment position interpolation
|
|||||||||
![]() |

Specifications
Specifications | Lathe system | Milling system | |
Control axes |
Max. number of axes (NC axes + spindles + PLC axes) | 6 | 6 |
Max. number of NC axes (in total, across all part systems) | 3 | 3 | |
Max. number of spindles | 2 | 1 | |
Max. number of PLC axes | 2 | 2 | |
Number of simultaneous contour control axes | 3 | 3 | |
Max. number of part systems | 1 | 1 | |
Least command increment | 0.1μm | ||
Least control increment | 1nm | ||
Max. program capacity | 230kB (600m) | ||
Max. PLC program capacity | 8,000 steps | ||
Display | 8.4-inch color TFT display | ||
HMI Customization function | NC Designer | ||
Connection to MITSUBISHI CNC machine operation panel | Available |
Inquiry
Customer Inquiries
Mitsubishi Electric Corporation