News Release Archives
Note that the releases are accurate at the time of publication but may be subject to change without notice.
FOR IMMEDIATE RELEASE No. 2704
Mitsubishi Electric to Launch SiC Module-Equipped CNC Drive Unit
Tokyo, October 29, 2012 - Mitsubishi Electric Corporation (TOKYO: 6503) announced today the launch of a drive unit equipped with a silicon carbide (SiC) power module for computerized numerical controllers (CNCs). The MDS-DM2-SPHV3-20080 is a multi-hybrid, multi-axis integrated-drive unit for drive control of spindle and servo motors. Sales will begin on December 3.

Power conversion modules are widely used in inverters and converters of household appliances and industrial equipment. SiC power modules are superior to conventional silicon (Si) modules in terms of their significantly reduced switching loss and high tolerance to temperature.

To date, Mitsubishi Electric has commercialized SiC power modules for inverters in air conditioners and railcars. The new SiC power module for CNC drive units offers higher speed and torque for driving machine tool spindles and servo motors, which is expected to improve manufacturing productivity in factories.


Power conversion modules are widely used in inverters and converters of household appliances and industrial equipment. SiC power modules are superior to conventional silicon (Si) modules in terms of their significantly reduced switching loss and high tolerance to temperature.

To date, Mitsubishi Electric has commercialized SiC power modules for inverters in air conditioners and railcars. The new SiC power module for CNC drive units offers higher speed and torque for driving machine tool spindles and servo motors, which is expected to improve manufacturing productivity in factories.

Main Features
SiC power module for higher speed and torque
|
|||||||||
![]() |
|||||||||
Power shut-off and other functions enable downsizing and reduced wiring
|
|||||||||
![]() |
|||||||||
Mitsubishi Electric's new CNC drive unit will be showcased at the 26th Japan International Machine Tool Fair (JIMTOF 2012), which will be held at Tokyo Big Sight in Japan from November 1-6. |
Specifications
Model name | MDS-DM2-SPHV3-20080 | |
Nominal maximum current for spindle (at peak)[A] | 200 | |
Nominal maximum current for servo (at peak) [A] | 80 x 3 axes | |
Output | Rated voltage [V] | 155AC |
Rated current for spindle [A] | 63 | |
Rated current for servo [A] | 15.8 | |
Input | Rated voltage [V] | 200 to 230AC Tolerable voltage fluctuation: Between 10% and -15% |
Rated current [A] | 60 | |
Control power | Voltage [V] | 24DC±10% |
Compatible spindle motors | SJ-V15-03ZT, SJ-V15-09ZT, SJ-V11-08ZT, SJ-DJ15/80-01, SJ-DL3.7/240, SJ-BG090D/300 |
|
Compatible servo motors | HF54, HF104, HF154, HF204, HF224, HF223,HF303, HF302 | |
Weight [kg] | 15 | |
Dimensions [mm] | W:260 x H:380 x D:278 |


Inquiry
Customer Inquiries
Mitsubishi Electric Corporation