BackPrint

News Release Archives

Note that the releases are accurate at the time of publication but may be subject to change without notice.

FOR IMMEDIATE RELEASE No.2681

Mitsubishi Electric Completes Installation of Japan's Largest Digital Signage Systems at Narita International Airport

Tokyo, June 26, 2012 - Mitsubishi Electric Corporation (TOKYO: 6503) announced today that it has completed installation of Japan's largest digital signage system at Narita International Airport, comprising a total of 100 display units made up of a total of 336 display panels, including Panorama Vision, an organic light-emitting display (OLED) screen. The system, which covers all passenger terminal areas, displays airport news, entertainment programs and advertisements as well as relaxing imagey, including "Living Japan", which depicts the beautiful natural scenery of Japan, and "Aquarium Japan," which shows enchanting marine life. Following an opening ceremony on June 26, 2012, the system will begin full-scale operations.

Narita International Airport has undertaken a fundamental review of airport information presentation and has introduced this digital signage system to deliver appropriate and timely information to its customers.

In addition to manufacturing the large display systems and the video streaming system, Mitsubishi Electric contributed to the overall concept design, including unit placement, design of the large display systems and LCDs, and video content creation, which includes choosing the clearest and most visually appealing fonts and progression speeds for each location and how to most effectively arrange displays to provide information and entertainment to waiting travelers.

Panorama Vision

Panorama Vision

Large-scale multiple LCD screen unit (27 panels)

Large-scale multiple LCD
screen unit (27 panels)


Core features of the system include
+Panorama Vision, the world's first seamless and smooth 160-degree OLED concave screen. It measures 9.6m x 1.9m (385-inch), consisting of 2,000 96mm x 96mm OLED panels.
+Large-scale multiple LCD screen units installed in all passenger terminal areas, including a 9.2m x 1.7m unit consisting of 27 46-inch display panels (equivalent to a 370-inch screen) as well as units made up of 16, 12, 8 and 4 panels, respectively.
+42-inch touchscreen user stations created along the principles of universal design.
+Mediaway, a video streaming system, delivering full HD video to 100 display units simultaneously or independently, and capable of promptly switching from scheduled videos to emergency information.
 
 
42-inch LCD touchscreen
42-inch LCD touchscreen
   55-inch LCD monitors
55-inch LCD monitors
 
 

Delivered systems

System nameSpecificationNumber of unitsLocation
Panorama VisionOLED Panorama Vision
9,600 mm x 1,920 mm
11PTB (Passenger Terminal Building)
South Wing 4th floor
International Departure Lobby
Large Display (type I)16 46-inch LCD multi panels11PTB, North Wing 4th floor
International Departure Lobby
Large Display (type II)4 46-inch LCD multi panels11PTB, North Wing 4th floor
International Departure Lobby
11PTB, South Wing 4th floor
International Departure Lobby
Safety Inspection Information Terminal12 46-inch LCD multi panels21PTB, North Wing 4th floor
Safety Inspection Area
21PTB, South Wing 4th floor
Safety Inspection Area
Arrival Information Terminal4 46-inch LCD multi panels21PTB, North Wing 1st floor
Arrival Lobby
21PTB, 4th floor
Arrival Lobby
Shop Information Terminal8 46-inch LCD multi panels31PTB, South Wing 1st floor
Restaurants and Shops Area
Complex Information Terminal27 46-inch LCD multi panels
9249mm x 1743mm
22PTB, 3rd floor
International Departure Lobby L
22PTB, 3rd floor
International Departure Lobby R
Welcome Information Terminal (type II)12 46-inch LCD multi panels12PTB, 1st floor
International Arrival Lobby L
12PTB, 1st floor
International Arrival Lobby R
Arrival Information Terminal (type II)4 46-inch LCD multi panels22PTB, 4th floor
International Arrival Lobby L
22PTB, 4th floor
International Arrival Lobby R
Shop Search Terminal42-inch LCD touchscreen111PTB/2PTB 4th floor
Shops Area
Digital Signage Terminal55-inch LCD monitor641PTB/2PTB
Center FacilityMEDIAWAY1Information-Communication Center Building

Inquiry