News Release Archives
Note that the releases are accurate at the time of publication but may be subject to change without notice.
Mitsubishi Electric Develops All-SiC Inverter with High Power Density
The module, which is rated at 1,200V/300A, incorporates a SiC MOSFET (metal oxide semiconductor field effect transistor) and SiC SBD (schottky barrier diode). To increase power density, electric current density must be increased by lower electric resistance, so Mitsubishi Electric developed low-resistance wiring by using direct lead bonding to connect power semiconductor chips directly to the main terminals, eliminating the use of conventional high-resistance aluminum lead wires.
To achieve high current density, low-loss (low-resistance) power chips also had to be used, but this required the application of high-speed protection circuits to prevent a large destructive current during short circuits. Mitsubishi Electric applied a SiC-MOSFET with a built-in current sensor function to its all-SiC power module and utilized a high-speed short-circuit-protection circuit, making it possible to use a low-resistance SiC-MOSFET even at a high current density. In so doing, the company successfully achieved a power density of 50kVA per liter by an inverter operation with an output of 156kVA.
While silicon (Si) has traditionally been used for power semiconductor devices, in recent years SiC has come to be widely considered as a promising next-generation material. Compared to Si, SiC has a critical electric field for breakdown that is about 10 times higher and enables the reduction of power loss, which contributes to fewer emissions of carbon dioxide. Furthermore, the reduction of power loss implies the reduction of cooling equipment, and contributes to overall downsizing and lightening of electronic components for automotive and industrial uses.
Mitsubishi Electric plans to further downsize inverters for commercial viability.