News Release Archives
Note that the releases are accurate at the time of publication but may be subject to change without notice.
FOR IMMEDIATE RELEASE No.2658
Mitsubishi Electric Develops Multi-Band Power Amplifier for Automatic Band Switching and Seamless Roaming
Tokyo, February 7, 2012 - Mitsubishi Electric Corporation (TOKYO: 6503) announced today it has developed a 3GPP-compliant, six-band power amplifier to enable automatic band switching and seamless international roaming with a single mobile device.

The unit's power-added efficiency rating of 40% is one of the world's highest for a multi-band power amplifier, and its package is among the world's smallest at 3mm x 3mm x 1mm, which will lead to mobile devices offering longer battery life and reduced size.

Mitsubishi Electric's six-band power amplifier addresses several important needs in wireless communication. The increase in wireless traffic due to proliferating smartphones requires mobile devices increasingly to locate and switch to available frequencies when other bands are overloaded. Automatic band switching is also necessary for international roaming. In addition, the use of multiple amplifiers, each dedicated to a certain frequency band, forces mobile devices to devote more space to additional circuitry.

The unit's power-added efficiency rating of 40% is one of the world's highest for a multi-band power amplifier, and its package is among the world's smallest at 3mm x 3mm x 1mm, which will lead to mobile devices offering longer battery life and reduced size.

Mitsubishi Electric's six-band power amplifier addresses several important needs in wireless communication. The increase in wireless traffic due to proliferating smartphones requires mobile devices increasingly to locate and switch to available frequencies when other bands are overloaded. Automatic band switching is also necessary for international roaming. In addition, the use of multiple amplifiers, each dedicated to a certain frequency band, forces mobile devices to devote more space to additional circuitry.
Key Features
1) | Six-band functionality in a conventionally sized package
|
||||||
![]() | |||||||
2) | Top-level power-added efficiency for a multi-band power amplifier
|
qBoost is a trademark of Quantance in the USA and 3GPP is a trademark of European Telecommunications Standards Institute.