BackPrint

News Release Archives

Note that the releases are accurate at the time of publication but may be subject to change without notice.

FOR IMMEDIATE RELEASE No.2647

Mitsubishi Electric Launches 1200V/50A Large-Type Dual In-line Package Intelligent Power Module

Tokyo, January 26, 2012 - Mitsubishi Electric Corporation (TOKYO: 6503) announced today the launch of the 1,200-volt large-type transfer-mold Dual In-line Package Intelligent Power Module (DIPIPM) Ver.4 (model PS22A79) with an industry-leading current rating of 50 amperes. Sales of the power module, designed for use in package air conditioners and other industrial motors, will begin on January 31.
PS22A79

PS22A79

To save energy and elevate performance, a wide variety of current ratings ranging between several amperes and hundreds of amperes are rapidly being adopted for inverter-based motor drive systems. DIPIPM, transfer molded intelligent power modules commercialized globally by Mitsubishi Electric in 1997, are widely used in inverter-equipped appliances such as air conditioners, refrigerators and washing machines, as well as inverter motor drive systems for industrial applications. Mitsubishi Electric's current 1,200V, Large-Type DIPIPM Ver.4 series with a current rating of 5-35 amperes, launched in 2008, is noted for helping to minimize inverter system size.

Product Features

Enlarged output and downsized motor control systems
The PS22A79 employs the newly developed sixth-generation IGBT (LPT-CSTBT: Light-Punch Trough Carrier Stored Trench-gate Bipolar Transistor), in which carrier storage is improved through cell pitch reduction and power loss is minimized through application of the thin wafer process. The model reduces power loss by 15% compared to the preceding fifth-generation IGBT.
Reduced power loss enables the current rating to be raised to 50 amperes, up from 35 amperes in the 1,200V/35A Large-Type DIPIPM Ver.4 PS22A78-E.
Lower production costs thanks to built-in temperature sensor
The model's built-in temperature sensor offers vastly improved linearity and precision compared to that of the existing PS22A78-E model, resulting in more efficient heat control.
Manufacturers will benefit from further downsizing of inverter systems, as well as reduced system costs.
Note:DIPIPM and CSTBT are registered trademarks of MITSUBISHI ELECTRIC CORPORATION.

Main Features

PS22A79
Collector-emitter voltage1,200V
Collector current50A
Precision of temp. sensor+/- 5 degree
Dimensions31.0 x 79.0 x 8.0 mm
(same as conventional 1200V Large-Type DIPIPM Ver.4)
Built-in chipsThree-phase inverter with driver
(6 IGBT chips、6 FWD chips、3 HVIC chips、LVIC chip)
Pin configurationThree-shunt open-emitter type

Lineup

5A10A15A25A35A50A  (new)
PS22A72PS22A73PS22A74PS22A76PS22A78-EPS22A79

Inquiry