News Release Archives
Note that the releases are accurate at the time of publication but may be subject to change without notice.
Mitsubishi Electric to Install Diamond Vision Displays at Saitama Stadium 2002
The North and South Side stands each will be given a Diamond Vision display. Measuring 23 m x 10 m, they will be 20 percent larger than the stadium's current display, or almost as large as a full tennis court. Incorporating the highest quality light-emitting diodes (LEDs) aligned vertically and horizontally in an 8mm dot pitch (see specifications below), the new screens are able to display full high-definition video content, yet they will consume 35 percent less energy than the current display.
Two Ribbon boards will be installed along the Main and Back Upper stands. Each will be 169.6 m long and 0.8m high. In addition, 29.2 m long Ribbon boards will be installed in front of the photographer areas along the North and South Side stands. Simultaneous control of all Ribbon boards will enable total coordination of audio-visual renderings in the stadium.
Outside the stadium, new 175-inch displays each measuring 3.84 m x 2.24 m will be installed at the South Entrance, which serves as the main entrance to the stadium. The displays feature high-luminance LEDs aligned in a 6.7 mm dot pitch, the highest resolution for outdoor devices in the country, and can be viewed clearly from as far as 2 m away in daylight.
Also, a 19.2 m long Ribbon board will be installed on the back of the South Side Stand Diamond Vision facing outside to provide information to visitors.
As an added feature, the operation console for all signage is highly easy-to-use, meaning that they also can be used for non-professional soccer tournaments and other events.
Mitsubishi Electric has installed more than 1,700 Diamond Vision displays globally since it installed the world's first full-color large display system at Dodger Stadium in Los Angeles in 1980. Going forward, Mitsubishi Electric will continue to expand its business in large displays for public stadia and other sports facilities.
Specifications of New Diamond Vision Screens at Saitama Stadium 2002
Type | Diamond Vision LED | Diamond Vision LED ODT-6 |
Installation areas | North and South Side stands | South Entrance |
Size | 23.552 m (w) x 10.24 m (h) 1,011 inches | 3.84 m (w) x 2.24 m (h) 175 inches |
Maximum Brightness | 5,000 cd/m2 | |
Brightness-Halving period | 50,000 hours or longer | |
Dot pitch | ![]() | ![]() |
8 mm | 6.7 mm | |
Pixel size (dots) | 2,944 (w) x 1,280(h) | 576 (w) x 336 (h) |
Number ofdisplays | 2 | 1 |
Installation date | March, 2013 | March, 2014 |
Type | Diamond Vision LEDerAd (Ribbon board) | ||
Installation areas | Main and Back Upper stands | In front of photographer areas on North and South Side stands | The back of South Side stand |
Size | 169.6 m (w) x 0.8 m (h) | 29.2 m (w) x 0.8 m (h) | 19.2 m (w) x 0.8 m (h) |
Maximum Brightness | 5,000 cd/m2 | ||
Brightness-Halving period | 50,000 hours or longer | ||
Dot pitch | ![]() |
||
25 mm | |||
Pixel size (dots) | 6,784 (w) x 32 (h) | 1,168 (w) x 32 (h) | 768 (w) x 32 (h) |
Number of displays | 2 | 2 | 1 |
Installation date | March, 2014 |