Factory Automation

Update : 2022/06/23

MAX Service Satisfied Co.,Ltd.

System Integration Partner

Tension Controller, Machine maker, Automation in automotive factory.

MITSUBISHI TENSION CONTROLLER

Roll-to-Roll control equipment

The Roll-to-Roll control equipment proposed by Mitsubishi Electric Corporation offers a capability for simple and efficient combination of FA equipment to expand the capacity of tension control.

While each product improves the productivity in each field, establishing a network environment improves the visualization of production lines.

Using Mitsubishi Electric FA equipment for the entire production and processing of a variety of long materials as film, textiles, and printable electronic maximizes the advantages.

Unwinding control

  • The figure right shows The outline of an unwinding control system that uses a powder brake.
  • Since unwinding tension equals braking torque divided by unwinding radius, tension can be kept constant by reducing the braking torque according to the decrease in reel daimeter.
  • A speed increaser and speed reducer such as gear are installed as necessary between the reel shaft and the powder brake.

Winding control

  • The figure right shows the outline of a 2-shaft switchover winding control system that has a servo motor.
  • This is an example of a feedback controlled tension control system based on the signals from the tension detector and in which pre-drive control for the auto feeder is also performed.

Roll to Roll Machine and Part

MAX Service ready to support every aspect Factory customer requirements. Products are ready
for immediate delivery to customers.

If customers need or even spare parts for customers to use during place an order. This makes customers no longer have to stop and wait.

There is also an option for customers who want to repair your device. We have spare parts service all the time. Confident in our products and services and will not be disappointed.

Machine maker

We are the machine maker and builders in automation Machine, Roll to Roll machine design to meet customer demand is our main job. Customers can request for advice.

By the way, we will manage until the customer is satisfied with comprehensive after-sales service
professional team.