Anywire is a wiring-saving system equipment manufacture and offers solutions for “diagnosis” of factory, “predictive/preventive maintenace” and “various traceability“ in partnership with Mitsubishi Electric e-F@ctory and IQSS.
I/O terminals to connect general purpose sensors and actuators with AnyWireASLINK network. Elimination of BOX can be promoted by increased downsizing including small I/O terminal of fingertip size allowing dispersion and terminal block type realizing compact size of volume ratio of 1/3 in comparison with conventional types. Available from 2 points to 32 points terminal. SmartASLINKER which is a kind of 2-point input I/O terminal can diagnose output line disconnection, power line short-circuit, power line disconnection and 0 volt line disconnection in real time while operating 2-wire and 3-wire type sensors. It provides strong support for prompt recovery of the system.
Anywire brand sensors which sensor function and I/O terminal function are combined in an identical sensor device can directly connect to transmission cable without any I/O terminal. It is an ultimate style of wiring-saving which you can not eliminate anything. Besides, preventive maintenance with the sensor is possible because not only ON/OFF status but also its sensing level can be monitored in real time. It also enable to reduce adjustment steps and man-hours by setting sensitivity, threshold and parameters at a upper controller or a display.
If you introduce ASLINKPOKAYOKE there is no need to look for parts with a list in one hand, and no errors occur in parts and quantity. In addition, these POKAYOKE terminals into which AnyWire’s unique wiring-saving technology is integrated offer many advantages such as freedom of installation, easy wiring work, flexibility in change and remodeling.
https://www.anywire.jp/en/pdf/catalog_ASLINKPOKAYOKE_1.1_E.pdf
< Increase in space efficiency by downsizing of I/O terminals >
Elimination of BOX can be promoted by increased downsizing including small I/O terminal of fingertip size allowing dispersion and terminal block type realizing compact size of volume ratio of 1/3 in comparison with conventional types.
< Whether sensor non-detection? or disconnection? can immediately be determined >
It was necessary for conventional I/O terminals to confirm whether sensor was in a non-detection state or whether sensor itself was in failure (sensor cable disconnection) for actual product. However, remote monitoring is allowed from upper controller and disconnected sensor is also easily identified by mounting this function. Disconnection detection function for sensor cable mounted on ASLINKER can significantly reduce time spent on investigation of cause. Monitoring is also facilitated by combination with GOT, and a highly visible monitoring system is allowed to be built.
< Diagnosing not only ON/OFF but also measured value for preventive maintenance >
Photoelectric sensor of ON/OFF operation etc., cannot actually determine ON far from OFF or ON close to OFF. ASLINKSENSOR allowing diagnosing of measured values can monitor its state from a upper controller, therefore, it can grasp the state of the sensor.
*ASLINKSENSOR always monitors sensing level of a sensor. The sensing level is converted into digital data, which is transmitted to a upper controller and is monitored by GOT, therefore, preventive measures such as replacement, adjustment and cleaning can be taken before “the sensor can be turned ON.”
< Collective change of sensitivity setting and reduction in adjustment production steps and man-hours by fine adjustment of threshold >
It was common to perform sensitivity setting of sensor and adjustment of threshold one by one on-site. However, ASLINKSENSOR allows collective setting changes of all sensors to be operated from a higher position. ASLINKSENSOR can also save set values. Therefore, it minimizes downtime such as at the time of setup change. In addition, this can prevent “momentary stop” before it happens during adjustment of threshold, and can control maintenance timing.
In the present robot control, various challenges have surfaced along with increasingly more intelligent and complex robot hands. AnyWireASLINK is the most advanced sensor wiring-saving system, as well as the most suitable robot wiring-saving system for resolving various challenges with more intelligent and complex robot hands.
Control of human errors in picking work is an essential element for enhancement and improvement in production of efficiency and product quality. Systems and devices to prevent such human-induced careless mistakes (poka) are called “POKA-YOKE”. “POKAYOKE” system based on AnyWireASLINK provides a solution to such problem simply and at low cost. There is no need to look for parts with a list in one hand, and no errors occur in parts and quantity. In addition, these POKAYOKE terminals into which AnyWire’s unique wiring-saving technology is integrated offer many advantages such as freedom of installation, easy wiring work, flexibility in change and remodeling, and dif culties in introduction can be lowered.