Factory Automation

Update : 2019/12/27

Panduit

Device Partner

Panduit is a world leader that engineers flexible, end-to-end electrical and network connectivity physical infrastructure solutions that help businesses stay connected in a global world.

Address
60 Tuas Avenue 11, Singapore 639106
Website
https://www.panduit.com/ Open new window

Fiber Optic and Copper Cabling Systems

Panduit’s extensive fiber optic and copper network cable product range offers great return value, guarantee future reliability, and provide the foundation for customer’s network growth. The network cablings ensure high performance, reliability, and scalability across the whole of customer’s mission critical physical network infrastructure. The advantages provided by Panduit’s fiber optic cabling options ensure uptime is maximized throughout the network. The full line of Panduit’s innovative copper products supports all of today's most common IP applications including PoE and Wireless technologies. See more of the product offerings in the following links.

Fiber Optic Cabling Systems Open new window

Copper Cabling Systems Open new window

Cabinets, Thermal Management, Racks & Enclosures

Panduit offers a full range of network cabinets, thermal management solutions, racks and enclosures for manufacturing floors, data centers, telecommunication equipment rooms, and enterprise cabling applications. Take full advantage of the extensive offerings to enhance network reliability, optimize space, while save on energy consumption for physical network deployment and operation. See more of these offerings in the following link.

Cabinets / Enclosures Open new window

Power, Environmental, & Connectivity Hardware

With the pervasive connectivity between devices and nodes, today’s IT and network operation is power intensive. Reducing power consumption n saves money while promoting the health of our planet. The key to an environmentally sustainable business strategy lies in regulating energy usage, achieving energy efficiency, and leveraging a reliable physical infrastructure. Panduit power distribution, environmental, and connectivity hardware products do these by improving availability, scalability, power, cooling efficiency, and product quality, while minimizes network downtime and increases data center productivity. See more of the innovative products from Panduit that is able to help achieve this vision in the following link.

Power, Environmental, & Connectivity Hardware Open new window

Safety Device - Absence of Voltage Tester

Safety and security must always be of top priority in activities involving risks. The continuous innovation by Panduit resulted in the creation of the Absence of Voltage Tester – VeriSafe. This enables anyone working on a cabinet to know whether the cabinet has been completely de-energised prior to opening the cabinet and commencing any work which involved any electrical risks.

VeriSafe Open new window

Safety Device - Data Access Port

Often, the requirement to work on live control cabinets like reprogramming a controller installed in the cabinet would involve opening of the cabinet to access the controller. This increases the electrical risks faced by the worker and also increases the risks of damage to the other components in the cabinet. The Panduit Data Access Port is an easy to install, purpose built physical access coupling interface which eliminates the need to open a cabinet to access the internal live components. The Data Access Port is customisable with a selection of interface modules (network ports, USB ports, power outlet) to suit the required needs of the user. See how the Data Access Port is able to address accessibility issue in live cabinets and enclosures in the following link.

Data Access Ports Open new window

Wire Routing, Management & Protection

Fiber optic and copper cable routing systems need to be effective in enabling the cables to be properly protected on premise during operation and while installation. The modular Panduit Wyr-Grid cable baskets and Fiber Runners eliminates the need to cut the routing systems to size and shape at site for installation. This mitigates risk of damage to the cable and at the same time provides a secure and well-ordered routing system for network cables at site.

Routing Systems Open new window

Wireless Environment and Equipment Monitoring System

Physical environment variables such as temperature, humidity, vibration, air pressure can have effects on equipment and also in the manufacturing environment. See how the Panduit Synapsense series of Wireless Monitoring System provides a simple, yet robust, solution that communicates and visualizes data in industrial applications in the following link.

Synapsense Wireless Monitoring System Open new window

Industrial Network Infrastructure

The rapid influx of smart equipment and connected devices that can communicate on an Industrial Ethernet Network is enabling manufacturers to significantly improve processes and performance. Designing for the manufacturing environment requires an intimate knowledge of industry standards to ensure the infrastructure supports various environments on the plant floor. See how Panduit’s extensive range of Industrial Network Infrastructure products enable a rugged and structured solution approach to ensure the durability and scalability of the manufacturing networks in the following links.

Industrial Network : panduit3d.com Open new window
https://www.panduit.com/en/solutions/industrial-networks-and-IoT.html Open new window

Enterprise Network Infrastructure

More Intelligent Networks for Enterprise Network convergence, building automation, and proliferating connected devices are shaping today's enterprises, placing new demands on the network and IT management staff. From the data center to telecom rooms and office environments, see how Panduit delivers highly-engineered, end-to-end cabling infrastructure and connectivity solutions that help move our customer’s business forward in the following link.

Enterprise Network Open new window

Data Center Network Infrastructure

Evolving technologies and increasing organizational demands for optimized agility and efficiency require increased visualization, automation, and high-performance networks of today’s complex data centers. Whether reconfiguring existing data center physical infrastructure or building from the ground up, see how Panduit’s data center solution is able to help achieve long term operational expense savings while maximizing physical infrastructure and cooling efficiency.

Data Center Network Open new window