A well experienced manufacturer and trader, combinding Mitsubishi Automation devices to adapt to any industrial applications, Specialise in Automation - We supply automatic machines for sheet metal processing tasks like Straightener Feeder, 2D, 3D Transfer robot and special MADE TO ORDER projects
This transfer robot is designed to support the 4.0 industry. Mitsubishi Electric played such a major role into making this product perfect. Controlled by HC-SFS202B Servo Motor with Motion CPU and PLC CPU
This metal sheet processing task machine feeds perfectly straight metal coil into the press machine. Making sure the mechanism runs smoothly, we use HA-LFS601B Servo Motor. Function setting has never been easier. Key operations and numeric vaules appear on a cutting edge GT1155-QSBD, Graphic Operation Terminal
This project was created in order to automate the “pick & place” process between one point to the next. To ensure the accuracy and efficiency, we use Mitsubishi Electric PLC (QD77MS4) which is programed for precise positioning control as well as Mitsubishi Electric Robot.
The project is a solution to reducing idel time between press machines in the production line. 3 Press machines all run in synchronized mode. This is made possible by QJ61BT11N CC Link Master and FANC-110 SBH CC Links
Core Business & Area Expertise:
PLC and Servo Implementation
Production Line and Positioning
Electrical Wiring