Amazon is a premier solutions provider for process and factory Automation. We are appointed by Mitsubishi Electric to be the Authorised System Integrator in Singapore. We specialise in integrating Mitsubishi Electric's World Class Programmable Logic Controllers, Drives, HMIs and SCADA systems for use in automation sectors, and also enables remote monitoring and control of these systems via secure virtual private network (VNP).
Mitsubishi Electric PLC controllers can easily integrate with other systems through its support of many popular open protocols which include CC-Link, Profibus, Modbus, Industrial Ethernet and DeviceNet.
Process & Factory Automation
This project is to automate the handling process of Cement Products from the vessels and deliver to various customers within the port.
In this complex fully automated process, a centralized SCADA System is used to monitor and control the operation process through Mitsubishi Electric’s PLCs being implemented at various locations.
Additionally, Mitsubishi Electric’s PLCs are also integrated with the Radio Remote Control Systems for Cranes Operational Control.
Filtration of waste water in a Petrol Chemical Plant
Amazon has various experiences on providing control systems design and engineering on: