• twitter
  • facebook
  • mail

Products

Print Page

 

MELSOFT RT ToolBox2

RT ToolBox2 Simulation

This PC software supports everything from system startup to debugging, simulation, maintenance and operation.
This includes Simulation and editing, operational checking before robots are installed, measureing process tact time,debugging during robot startup, monitoring robot operation after startup, and trouble shooting.

3D Viewer

  • Graphical representation of a work along with the dimensions, color and other specified details of the work area to be gripped.
  • Hands can be created as combinations of basic diagrams on the Hand Editing screen and then attached to the robot.
  • Standard 3D polygonal models (applicable 3D data file formats: STL,OBJ) can be imported into the program, allowing operators to confirm the relationshipamong the hands, workpieces, and peripheral devices during simulation.
(*It can not be used with the mini edition.)

3D viewer,modeling

Enhanced visual functions

  • Enhanced RT ToolBox2 (PC software) graphic display function allowing setting parameters to be displayed visually.
    Visual confirmation using this function helps to proactively prevent setting errors.
  • Display of teaching positions and trajectories of end points helps to facilitate confirmation tasks during programming or simulations.
(*It can not be used with the mini edition.)

Enhanced visual functions

Simulation function

  • Offline robot motion and tact time check for designated parts of a program.
(*The simulation function only supports the "RT ToolBox2" standard edition. It can not be used with the mini edition.)

Simulation

Spline curve

  • It is possible to create and edit a spline file for using the spline interpolation function.
  • The spline curves and selected position data are displayed in the 3D monitor.
  • It is possible to create a robot program using a path point data registered in the spline file or capture the position data of the robot program as a route point data of spline file.
  • If opened a spline file corresponding to the Ex-T spline, spline curve will be displayed in the start position was along the Ex-T coordinate position.
(*The spline function can be used with Version S5/R5 or later of the robot controller software.)

Spline curve

Save AVI

It is possible to record contents in the 3D monitor and save the AVI file.(version 3.20W or later)

(*It can not be used with the mini edition.)