Factory Automation

Human-Machine Interfaces (HMIs)-GOT FA Application Package iQ Monozukuri

iQ Monozukuri Process Remote Monitoring Easily introduce IoT technologies to the shop floor

Easily implement iQ Monozukuri Process Remote Monitoring system

System configuration example

System configuration example
  • *1Up to five GOTs can be managed for each license. To manage information of 50 GOTs, purchase the product including 10 licenses.
Mitsubishi Electric FA application package
(1) iQ Monozukuri Process Remote Monitoring Process Remote Monitoring setting tool
iQ Monozukuri Process Remote Monitoring template project for GT SoftGOT2000
Products to be prepare by users (Required)
(2) Personal computer + display
or MELIPC MI3000
A personal computer to run the software necessary for iQ Monozukuri Process Remote Monitoring.
(3) GT SoftGOT2000 Software to display processes monitoring and analysis results of resource data on the personal computer screen. The software is included in HMI/GOT Screen Design Software GT Works3.
(4) GT SoftGOT2000 license key License key to use GT SoftGOT2000. When using MELIPC MI3000 (see (2)), the license key is pre-installed so that it is not required to purchase separately.
(5) GT Designer3 Software to create or change an iQ Monozukuri Process Remote Monitoring template project for GT SoftGOT2000 and on-site GOT project files. The software is included in HMI/GOT Screen Design Software GT Works3.
(6) GOT2000 GT27, GT25, GT23, GT21, and GS21 models with an Ethernet port can be used.
Products to be prepare by users (Optional)
(7) Data storage Required to use resource interaction or operator information management of iQ Monozukuri Process Remote Monitoring functions.
(8) Devices such as programmable controller or drive equipment Provides information of shop floor such as operating time, production quantity, and operating conditions to on-site GOTs. Models that support a communication driver of an on-site GOT can be used.
(9) Network camera, etc. Used to check the on-site conditions by video.
(10) VNC server function license License necessary to browse on-site GOT screens via a personal computer which uses this application package.
(11) GOT Mobile function license License necessary to browse on-site GOT Mobile screens via a personal computer which uses this application package.
(12) Mobile terminal Required when using the working memo function of the Pocket GOT mobile app for Android™OS or iOS®.
(13) Others Prepare necessary items depending on the devices and functions to be used (browsers to display camera images or display web pages, user-created applications, etc.).

Data flow and each purpose

Data flow and each purpose
  • (A)On-site GOTs collect data of connected devices.
  • (B)The mobile app sends the information entered with the working memo function to the on-site GOTs.
  • (C)Process Remote Monitoring setting tool collects data collected by on-site GOTs.
  • (D)The data collected by Process Remote Monitoring setting tool is displayed in GT SoftGOT2000.
  • (E)GT SoftGOT2000 outputs collected resource data files or starts other applications.