MELSERVO-J5 Series Rotary Servo Motor Model Designation
![](/fa/products/assets/img/img_mv-1_sm.jpg)
- HK-KT Series (Low Inertia, Small Capacity)
- HK-MT Series (Ultra-Low Inertia, Small Capacity)
- HK-ST Series (Medium Inertia, Medium Capacity)
- HK-RT Series (Ultra-Low Inertia, Medium Capacity)
- Related Link
HK-KT Series (Low Inertia, Small Capacity) (Note 2)
![Model Designation HK-KT Series](./assets/img/motor.jpg)
- Notes:
- 1. The dimensions are the same regardless of whether or not an oil seal is installed.
- 2. This section describes what each symbol in a model name indicates. Some combinations of symbols are not available.
- 3. A geared servo motor with an oil seal installed is not available.
- 4. The dimensions of the servo motors with functional safety are the same as those of the standard servo motors.
HK-MT Series (Ultra-Low Inertia, Small Capacity) (Note 2)
![Model Designation HK-MT Series](./assets/img/motor_04.jpg)
Notes:
- 1. The dimensions are the same regardless of whether or not an oil seal is installed.
- 2. This section describes what each symbol in a model name indicates. Some combinations of symbols are not available.
- 3. The dimensions of the servo motors with functional safety are the same as those of the standard servo motors.
HK-ST Series (Medium Inertia, Medium Capacity) (Note 2)
![Model Designation HK-ST Series](./assets/img/motor_02.jpg)
- Notes:
- 1. The dimensions are the same regardless of whether or not an oil seal is installed.
- 2. This section describes what each symbol in a model name indicates. Some combinations of symbols are not available.
- 3. The standard HK-ST G1/G1H servo motors have a keyed shaft (with a key).
- 4. A geared servo motor with an oil seal installed is not available.
- 5. The dimensions of the servo motors with functional safety are the same as those of the standard servo motors.
HK-RT Series (Ultra-Low Inertia, Medium Capacity) (Note 2)
![Model Designation HK-RT Series](./assets/img/motor_03.jpg)
- Notes:
- 1. The dimensions are the same regardless of whether or not an oil seal is installed.
- 2. This section describes what each symbol in a model name indicates. Some combinations of symbols are not available.
- 3. The dimensions of the servo motors with functional safety are the same as those of the standard servo motors.